I am trying to connect my wifi to access point but i am getting below error in the serial terminal after pressing the reset button
my boards are MIMXRT1060- EVK and AW-NM191-uSD
Starting webconfig DEMO
[i] Trying to load data from mflash.
[i] Nothing stored yet
[i] Initializing WiFi connection...
[wifi_io] Error: Error in wlan_card_status()
[wifi_io] Error: Card timeout wlan_download_normal_fw:362
[wifi] Error: sd_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1
Solved! Go to Solution.
suggest to terminate debug sessions and unplug Dut and restart again.
suggest to terminate debug sessions and unplug Dut and restart again.
Yes , I have done this same step but same error is come
Could you please make sure that you modified the module to use in the setting of the project ?
regards
Thanks for your help, Due to module connection issue we got this error . now it is working properly