Radio Range for JN5168-001-M00

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radio Range for JN5168-001-M00

1,416 Views
davidashraf
Contributor V

Hello , 
I am new to JN516x Zigbee Pro development ,and I want to know what is the maximum distance between 2 modules  (JN5168-001-M00) that cannot be exceeded for proper communication between the 2 modules.
Also I want to know whether there's a way to control this maximum range through Software.
 
Thanks.

4 Replies

835 Views
limcb
Contributor IV

It is short.

Indoor, about 1 room away but If you chose the JN5169 (if there is module version) or JN5168-M05 version, the range should be a lot further. 

Please use this find JN-AN-1172 JN516x-Customer-Module-Evaluation-Tool, to test the range.

Please use Channel 25 / 26, to ensure no WiFi interference for Maximum Range.

You'll also need to know/set what is your maximum allowable PER at 'maximum range'. 

From datasheet,

JN5168-M00 > Transmit power  2.5 dBm

JN5169-M00 > TX power 8.5 dBm/10 dBm

JN5168-M05 > Transmit power  9.5 dBm

835 Views
adamjacob
Contributor II

Calling the makers and experts using Zigbee via NXP JN5168 modules, please join the facebook group so we can help each other:)
https://goo.gl/DeYbC6 
Cheers

835 Views
davidashraf
Contributor V

adamjacob‌ 
Thanks for sharing! 

0 Kudos

835 Views
davidashraf
Contributor V

Do both modules ( JN5169-M00 , JN5168-M05 ) need external antennas to achieve this Tx power ( 10 dbm , 9.5 dbm )
or this power is achieved by the on boar
d antenna ??

Also If I used a module ( 
JN5169-001-M06 ) having receiving sensitivity of -100 dbm , for how much could this enhance the radio range ? 

Thanks

0 Kudos