Hi,
I am now using RF4CE for device docking, and I find that my remoter can only be matched with up to 8 receiver, even if I set
#define RF4CE_NWKC_MAX_PAIRING_TABLE_ENTRIES 10
#define RF4CE_NWKC_MAX_NODE_DESC_LIST_SIZE 10
What should I do if I want to increase the number of pairing?
The device is jn5168, SDK is JN-SW-4060.
Hi @854648943,
The values, that you are trying to modify, are Constants explicitly defined by the ZigBee RF4CE Specification.
The RF4CE is not suported. Please look at the Zigbee 3.0 Stack.
Regards,
Mario
Hi @mario_castaneda ,
For some reason, i can't use zigbee 3.0, I can only use the RF4CE protocol, Our goal is to be able to set the maximum number of pairs to more than 10, which is very important to us. Is there any solution? Thank you very much.
Regards,
hantianheng
Hi @854648943,
I hope you are doing great.
The Zigbee Spec mention the max pairing table entries.
In this case, is 8, unfortunately, the stack is not longer supported.
Sorry for any inconvenience that this may cause you.
Regards,
Mario
Hi,@mario_castaneda
Thank you for your reply.
Do you mean that the maximum number can only reach 8 in NXP's RF4CE SDK, even if I set
#define RF4CE_NWKC_MAX_PAIRING_TABLE_ENTRIES 10
Regards,
hantianheng