QN9090 - working with SDCARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9090 - working with SDCARD

736 Views
shai_b
Senior Contributor II

Hello Team,

My customer needs to implement SDCARD but he did not found any material to perform such SD card implementation with the QN9090 Dev kit.

please advise if there is an example code to add an SD card or can you guide us to implement an SD card?

second thing, the customer wanted to know if PWM output can be set to be a logical 1 of V-REF/BIAS/BAND GAP (for example if the PWM can be at peak 2.5v)? 

please advise back, Thanks in advance 

Kind regards,

Shai

Labels (1)
  • QN

Tags (2)
0 Kudos
3 Replies

642 Views
shai_b
Senior Contributor II

Hello team,

I did not hear from you for a while, I would really appreciate your support in #SDcard implementation with #QN9090 device.

Thanks in advance 

kind regards,

shai.b@telsys.co.il

0 Kudos

642 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Shai,

I hope you are doing great.

please advise if there is an example code to add an SD card or can you guide us to implement an SD card?

 Unfortunately, we do not provide any support with the SD Card. However, you could use the SPI or I2C example for a better reference for the customer implementation.

second thing, the customer wanted to know if PWM output can be set to be a logical 1 of V-REF/BIAS/BAND GAP (for example if the PWM can be at peak 2.5v)? 

The PWM output could be 2.5V depending on the VDDE. 

VDDE — Supply voltage for IO

pastedImage_2.png

Regards,

Mario

642 Views
shai_b
Senior Contributor II

Mario,

Thank you.

0 Kudos