QN9090 persistent storage options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9090 persistent storage options

Jump to solution
927 Views
MikeCalm
Contributor II

Hi All,

I wonder what are the best options to have persistent storage for QN9090.

As there is no EEPROM, the only way is using one or a few of the FLASH sectors.

I can't find any sample code for data storage.

Or .. Should I use external EEPROM?

 

Thanks,

Mike

 

0 Kudos
1 Solution
917 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi MikeCalm,

   About the internal flash operation, we have the SDK which contains the flash_demo, that project will help you to finish the flash program, erase, read operation.

   You can download the SDK code from this link:

https://mcuxpresso.nxp.com/en

  Choose board as QN9090DK6 , and download SDK_2.6.1_QN9090DK6.

  You can find the flash code in folder:

SDK_2.6.1_QN9090DK6\boards\qn9090dk6\driver_examples\flash

    But, as you know , the on chip flash has the endurance limit:

image.png

 

If your eeprom data is write frequently, I suggest you to use the external EEPROM with I2C interface.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
901 Views
MikeCalm
Contributor II

Hi Kerry,

Many thanks. Everything works as expected.

Best Regards,

Mike

0 Kudos
918 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi MikeCalm,

   About the internal flash operation, we have the SDK which contains the flash_demo, that project will help you to finish the flash program, erase, read operation.

   You can download the SDK code from this link:

https://mcuxpresso.nxp.com/en

  Choose board as QN9090DK6 , and download SDK_2.6.1_QN9090DK6.

  You can find the flash code in folder:

SDK_2.6.1_QN9090DK6\boards\qn9090dk6\driver_examples\flash

    But, as you know , the on chip flash has the endurance limit:

image.png

 

If your eeprom data is write frequently, I suggest you to use the external EEPROM with I2C interface.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 Kudos