QN9090/9030 Mesh

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,425件の閲覧回数
Nxpfan
Contributor I

Hi Does QN9090/QN9030 sdk support ble mesh? If yes, then how to get demo and lib? If no, does NXP have plan to support ble mesh in QN9090/9030 sdk?

Thanks,

0 件の賞賛
1 解決策
1,371件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

We have not developed the zigbee sdk. So it can only used the ble. If you want to use mesh network, we recommend the K32W061.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
1,407件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The QN9090 ble can connect to up to 16 device at the same time in theory. But it is not convenient to organize the network compared with zigbee. And we do not have the sdk to realize the multiple connection.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
1,397件の閲覧回数
Nxpfan
Contributor I

Hi TIC,

Thanks for reply. From nxp post: https://media.nxp.com/news-releases/news-release-details/nxp-delivers-new-bluetooth-microcontroller-...

it states QN serials has ble support. Does it mean NXP have plan to support ble mesh sdk?

Does any other nxp product support ble mesh?

Thanks,

タグ(1)
0 件の賞賛
1,388件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

mesh network (or simply meshnet) is a local network topology in which the infrastructure nodes (i.e. bridges, switches, and other infrastructure devices) connect directly, dynamically and non-hierarchically to as many other nodes as possible and cooperate with one another to efficiently route data from/to clients. The ble do not support. The qn9090 support the 802.15.4 that the zigbee rely on. So the zigbee is more suitable to support the mesh network.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
1,379件の閲覧回数
Nxpfan
Contributor I

Hi TIC,

ok, then  BLE mesh(or bluetooth SIG mesh) is not supported on QN9090/9030 SDK. You mentioned "The qn9090 support the 802.15.4 that the zigbee rely on" , so does QN9090 SDK  support zigbee feature already or is there any document about qn9090 zigbee information?

 

Thanks,

0 件の賞賛
1,372件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

We have not developed the zigbee sdk. So it can only used the ble. If you want to use mesh network, we recommend the K32W061.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛