Can part QN9090-001-M10 be ordered somewhere? I see the QN9090-001-T10 on digikey (out of stock of course) but cannot find the -001-M10. The T10 has the mezzaninne board with connectors which I don't need/like.
Additionally, is the QN9090-001-M10 FCC certified? How about the QN9090-001-T10 ?
Yohst...California Eastern Laboratories has a certified module based on the QN9090 chip set. The module is on an interposer board that plugs into NXP's QN9090-DK-006; it's similar to their QN9090-001-T10. You can also work with the loose module (not pluggable...castellation edge connections instead that need to be soldered). Send me a private email and I can share more details and we can see if it's a fit for your design.
https://www.cel.com/product/cbt250/
Regards-Bruce Havemeier