Has any one tested QN908x HID USB interface on a MAC OS. When I tried it on MAC OS it doesn't seems to recognize, the same version of the HID USB example project works on the system which is loaded with Windows 10 OS. kindly let me know if there is any specific protocol support need to be added to make it working in MAC OS. Regards, kishan
ok @Ricardo_Zamora.
Let me know if anyone else tested/ tried the NXP QN908x USB HID example application on a MAC OS, and if so please let me know the outcome.
-kishan
Hi,
Hope you are doing well. We do not have examples that work with MAC OS. You can take the USB HID Generic example as a base, but you will need to adapt it to the needs and with the necessary features to make it work on that OS.
Regards,
Ricardo
Hi @Ricardo_Zamora ,
Thanks for the update, would like to know where can I look for the feature specification in order to make the QN908x USB HID work on MAC OS.
Hi,
For this information, you should go with that company, to get the USB specification to work with the OS of their machines.
Regards,
Ricardo