QN9080 - issue with CRP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9080 - issue with CRP

1,096 次查看
maxasaulov
Contributor II

Hi,

I'm trying to enable CRP2 for the device based on QN9080. According to the https://www.nxp.com/docs/en/nxp/user-guides/UM11023.pdf (page 73) CRP is controlled by 4 bytes at 0x20 offset in the vector table.  Here is the hex dump of firmware vector table that I'm flashing

> hd firmware.bin | head

00000000 f0 ff 01 04 f1 1b 00 00 59 1d 00 00 69 1d 00 00 |........Y...i...|
00000010 69 1d 00 00 69 1d 00 00 69 1d 00 00 00 00 00 00 |i...i...i.......|
00000020 fe 68 06 00 00 00 00 00 00 00 00 00 69 1d 00 00 |.h..........i...|
00000030 69 1d 00 00 69 1d 00 00 69 1d 00 00 69 1d 00 00 |i...i...i...i...|‍‍‍‍

There is 0x000668fe at 0x20 which is mentioned on page 84 as the default value for CRP2.

After flashing I've shorted the CHIP_MODE pin to the ground and connected the USB - new mass device appeared with the name "CRP DISABLD". I've also downloaded the firmware from the device using JLink. Here is the hex dump 

> hd downloaded.bin | head

00000000  f0 ff 01 04 f1 1b 00 00  59 1d 00 00 69 1d 00 00  |........Y...i...|
00000010  69 1d 00 00 69 1d 00 00  69 1d 00 00 22 51 fd fb  |i...i...i..."Q..|
00000020  ff a8 0a 00 00 00 00 00  00 00 00 00 69 1d 00 00  |............i...|
00000030  69 1d 00 00 69 1d 00 00  69 1d 00 00 69 1d 00 00  |i...i...i...i...|

You can see that value at 0x20 changed to 0x000aa8ff which is the default value for no CRP.

Any ideas whats wrong?

SDK: SDK_2.2_QN908xCDK_Beta
IDE: mcuxpressoide-10.0.2_411
System : Ubuntu 16.04

Regards,
Max.

标签 (1)
标记 (4)
2 回复数

701 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Max,

If you are using JLink debugging interface you need to change the Device to "QN9080C (allow CRP)" in the debug configuration so that it allows you to write the CRP register. You need to manually add the quotation marks "" around the device name, so that it is passed correctly as a parameter to the JLinkGDBServer.

Run>Debug Configurations...

pastedImage_2.png

With this change to the debug configuration I was able to change the CRP to 0x000668FE and the USB ISP bootloader enumerates as "CRP ENABLD".

pastedImage_5.pngpastedImage_6.png

Additionally, the RFP (Ready for Production) build of the QN9080 SDK is now available from the MCUXpresso SDK builder and some new tools are also available in the Lab and Test Software section of the SOFTWARE & TOOLS tab in the QN908x product page.

Let me know if this works for you.

Regards,

Gerardo

701 次查看
maxasaulov
Contributor II

Hi Gerardo Rodríguez,

Yes, it works. Thanks.

Regards,
Max.