Dear NXP Support Team,
I am currently working with 88W8887 and require assistance with Access Point mode.
When a STA device connected to the access point is disconnected, the STA device issues a 'Disassociate'.
Is there a way to notify when this 'Disassociate' is issued?
Additionally, is there a way to issue a disconnection notification when the connection between AP and STA is severed by issuing this "Disassociate"?
I am using "SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p64-15.100.19.p64-C4X15704_A2-MGPL".
・Linux Kernel Version v3.18.24
・hostapd Version:2.10
・wpa_supplicant Version:2.10
I would greatly appreciate your guidance on the following points:
Are there specific configurations or settings required for the TCC8971(Telechips) to operate in AP mode effectively with the Marvell 88W8887 WiFi device?
Are there any firmware updates or specific versions that support AP mode more reliably?
Any additional troubleshooting steps or tools that I can use to diagnose and resolve the connection issues?
Thank you for your time and assistance,
Best regards,
Hiroyuki Kohchi
解決済! 解決策の投稿を見る。
Hi, @Pioneer
Thanks for creating case to us.
Please see my inline reply:
1. Is there a way to notify when this 'Disassociate' is issued? Is there a way to issue a disconnection notification when the connection between AP and STA is severed by issuing this "Disassociate"?
==>Sorry for the inconvenience. Currently, from controller side, we do not have such kind of policy which can automatically report/notify to end users when the connected STA disconnected with our 88W8887 working in AP mode. You can check related dmesg logs, journal log, or Wi-Fi OTA logs. According to the logs implement the requirement in application layer by yourself.
Are there specific configurations or settings required for the TCC8971(Telechips) to operate in AP mode effectively with the Marvell 88W8887 Wi-Fi device?
==>For Linux platform, you can refer to Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual
For Android platform, you can refer to: Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Android 14 OS
Are there any firmware updates or specific versions that support AP mode more reliably?
==>Our latest release is: SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p69-15.100.19.p69-CS4X15711_A2-MGPL
You can download it through above link and update your FW. We always suggest customer to use latest release because it includes some known fixes and has better compatibility.
Any additional troubleshooting steps or tools that I can use to diagnose and resolve the connection issues?
==>You can refer to Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual.
In section 3 Wi-Fi driver debugging, it includes some guide steps for Wi-Fi debug.
And specially for connection issues, we usually capture dmesg, wpa_supplicant journal logs and Wi-Fi OTA logs to see what happened.
On Linux terminal, directly execute: dmesg > log.log
It will save the dmesg logs into log.log file and saved on your host platform.
How to capture wpa_supplicant journal logs:
You can use below steps to enable the supplicant logs:
1. boot up the board
2. killall wpa_supplicant
3. open "vi /lib/systemd/system/wpa_supplicant.service"
4. add -ddd at end "ExecStart=/usr/sbin/wpa_supplicant -u -ddd"
5. reboot the board
6. Run the scenario using nmcli
7. run journalctl -a -b to capture the supplicant logs
To resolve connection issue, we need to identify what's the root cause, is from our side or from remote side. From driver side or FW side. Our Wi-Fi chip side or your application side. Anyway, once we find any evidence shows that the issue is from our Wi-Fi side, we will try to fix it. And you do not need to do anything except validation.
Please feel free to create case if need our support on our Wi-Fi chips.
Best regards,
Christine.
Dear Christine,
The recommendations for both Linux and Android platforms, along with the information about the latest firmware release, have been very helpful. I will proceed with updating the firmware and reviewing the recommended troubleshooting documents.
Thank you also for the instructions on log capturing and diagnosing connection issues. I will definitely refer to them.
Once again, I would like to express my gratitude for your thorough support. I look forward to your continued assistance should I need further help in the future.
Best regards,
Hiroyuki Kohchi
Hi, @Pioneer
Thanks for your feedback and you are always welcome.
If no other concerns on this case, would you mind mark my previous reply as a solution? So that we can close this case.
Please feel free to create new case to us if you have any other questions in the future.
Have a nice day~
Best regards,
Christine.
Hi, @Pioneer
Thanks for creating case to us.
Please see my inline reply:
1. Is there a way to notify when this 'Disassociate' is issued? Is there a way to issue a disconnection notification when the connection between AP and STA is severed by issuing this "Disassociate"?
==>Sorry for the inconvenience. Currently, from controller side, we do not have such kind of policy which can automatically report/notify to end users when the connected STA disconnected with our 88W8887 working in AP mode. You can check related dmesg logs, journal log, or Wi-Fi OTA logs. According to the logs implement the requirement in application layer by yourself.
Are there specific configurations or settings required for the TCC8971(Telechips) to operate in AP mode effectively with the Marvell 88W8887 Wi-Fi device?
==>For Linux platform, you can refer to Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual
For Android platform, you can refer to: Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Android 14 OS
Are there any firmware updates or specific versions that support AP mode more reliably?
==>Our latest release is: SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p69-15.100.19.p69-CS4X15711_A2-MGPL
You can download it through above link and update your FW. We always suggest customer to use latest release because it includes some known fixes and has better compatibility.
Any additional troubleshooting steps or tools that I can use to diagnose and resolve the connection issues?
==>You can refer to Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual.
In section 3 Wi-Fi driver debugging, it includes some guide steps for Wi-Fi debug.
And specially for connection issues, we usually capture dmesg, wpa_supplicant journal logs and Wi-Fi OTA logs to see what happened.
On Linux terminal, directly execute: dmesg > log.log
It will save the dmesg logs into log.log file and saved on your host platform.
How to capture wpa_supplicant journal logs:
You can use below steps to enable the supplicant logs:
1. boot up the board
2. killall wpa_supplicant
3. open "vi /lib/systemd/system/wpa_supplicant.service"
4. add -ddd at end "ExecStart=/usr/sbin/wpa_supplicant -u -ddd"
5. reboot the board
6. Run the scenario using nmcli
7. run journalctl -a -b to capture the supplicant logs
To resolve connection issue, we need to identify what's the root cause, is from our side or from remote side. From driver side or FW side. Our Wi-Fi chip side or your application side. Anyway, once we find any evidence shows that the issue is from our Wi-Fi side, we will try to fix it. And you do not need to do anything except validation.
Please feel free to create case if need our support on our Wi-Fi chips.
Best regards,
Christine.