PNEV5190 not listed in MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PNEV5190 not listed in MCUXpresso

ソリューションへジャンプ
1,216件の閲覧回数
Cousin63
Contributor I

Hi,

following PNEV5190B evaluation board quick start guide, at some time it is needed to install the SDK. Both in MCUXpresso / Installed SDK / Available Boards and on https://mcuxpresso.nxp.com/en/select, there is not board related to 5190.

There is an SDK_2_8_0_FRDM-K82F.zip (release date 2020-07-21), which has reference for 3 boards frdmk82f, frdmk82f_clrc663, frdmk82f_pn5180.

=> Is there a dedicated pn5190 SDK somewhere?

=> If not, should I use frdmk82f_pn5180?

Regards,

0 件の賞賛
1 解決策
1,206件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Cousin63 :

No, currently there is no dedicated package for PN5190.

For PN5190, you need to download SDK_2_8_0_FRDM-K82F.zip.

and import SDK_2_8_0_FRDM-K82F.zip into workspace, and together with nxpnfcrdlib

 

Regards

Daniel

 

元の投稿で解決策を見る

3 返答(返信)
1,207件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Cousin63 :

No, currently there is no dedicated package for PN5190.

For PN5190, you need to download SDK_2_8_0_FRDM-K82F.zip.

and import SDK_2_8_0_FRDM-K82F.zip into workspace, and together with nxpnfcrdlib

 

Regards

Daniel

 

1,117件の閲覧回数
StefanC
Contributor I

Hi, 

which of the 3 options do I need to pick for the pnev5190 since there is no dedicated package?

frdm82_f

clrc663

pn5180

 

0 件の賞賛
1,112件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

PN5190 reader library can be download from below link

https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NF...

PN5180 is a front end. can work with Frdm-k82f,  sdk for K82f can be downloaded from below link

https://mcuxpresso.nxp.com/en/welcome

Regards

Daniel

 

 

Regards

Daniel

0 件の賞賛