PN5180 acting as a card and as a reader simultaneously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5180 acting as a card and as a reader simultaneously

692 次查看
Matthias-A
Contributor II

Hi

I have a question about the PN5180. I was wondering whether it is possible to combine the HCE example and the discovery loop sample so that 1 PN5180 front end acts both as reader and as card. Or isn't that possible at all? 

 

Thank you

Matthias

0 项奖励
2 回复数

681 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, it's impossible. Pn5180 can't be used as both a card simulation and a reader simultaneously.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励

597 次查看
Matthias-A
Contributor II

Hi

Is is possible to multiplex both technologies in time. For instance: switching every 200 ms between HCE and reader? Or would that create compile problems since both technologies could not be compiled together?

Thanks

0 项奖励