PN5180 MIFARE CLASSIC Card unresponsive

cancel
Showing results for 
Search instead for 
Did you mean: 

PN5180 MIFARE CLASSIC Card unresponsive

169 Views
Matthias-A
Contributor II

Hi

I am developing with the PN5180 and a MIFARE CLASSIC card. I was testing the functionality of the nfc counter by authenticating multiple times with a wrong password. The card is probably blocked because of the wrong authentications but I was wondering whether or not I am able to recover the card in this situation or when the password is forgotten. Is it possible to recover in some way by completely erasing the card or something?

 

Thank you in advance

0 Kudos
1 Reply

157 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Matthias-A ,

 

Actually there is no command for such kind of function. Can the card be accessed with the right password?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos