Hello NXP TechSupport,
I am using PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p81-17.26.1.p81-MXM5X17277_V0V1-MGPL.zip package.
After loading the driver sometimes I am facing below error on wlp5s0f0 or wlp5s0f1
Error
------------------
$ ifconfig wlp5s0f0 up
$ ifconfig wlp5s0f1 up
$ iwlist wlp5s0f0 scan | grep SSID
wlp5s0f0 Interface doesn't support scanning : Operation not supported
OR
$ iwlist wlp5s0f1 scan | grep SSID
wlp5s0f1 Interface doesn't support scanning : Operation not supported
------------------
Also mlan0 OR uap0 interfaces availability is not consistent.
Then after retying unloading and reloading Driver few times fixes the issue.
What is the possible root cause for such random behavior ?
Kalpesh
------------------------------------------------------------------------------------------
Linux Driver Unload/Load log
-----------------------------------------
wlan: Unloading MWLAN driver
Free module params
Free module params
wlan: Driver unloaded
wlan: Loading MWLAN driver
Attach moal handle ops, card interface type: 0x206
PCIE9098: init module param from usr cfg
card_type: PCIE9098, config block: 0
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode = 7
ps_mode = 2
auto_ds = 2
fw_name=nxp/pcieuart9098_combo_v1.bin
rx_work=1 cpu_num=4
Request firmware: nxp/pcieuart9098_combo_v1.bin
WLAN FW is active
wlan: version = PCIE9098--17.68.1.p81-MXM5X17277-GPL-(FP68)
Attach moal handle ops, card interface type: 0x206
PCIE9098: init module param from usr cfg
card_type: PCIE9098, config block: 1
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode = 7
ps_mode = 2
auto_ds = 2
fw_name=nxp/pcieuart9098_combo_v1.bin
rx_work=1 cpu_num=4
Request firmware: nxp/pcieuart9098_combo_v1.bin
WLAN FW is active
wlan: version = PCIE9098--17.68.1.p81-MXM5X17277-GPL-(FP68)
wlan: Driver loaded successfully
OK! Thanks!@kbpanchal05 ,
Let us try to add interface name when loading driver.
attachment is configruation file for loading driver, all parameters for loading driver are in it. you can copy it to /lib/firmware/nxp, and use it like below:
===========Loading 9098 driver======
# insmod mlan.ko
# insmod moal.ko mod_para=nxp/wifi_mod_para.conf
================================
Then run ifconfig -a to check interface name.
---For MAC0: WiFi 6 802.11ax
Station is : mlan0
AP is : uap0
WiFi direct is : wfd0
---For MAC1 : WiFi 5 802.11ac
Station is : mmlan0
AP is : muap0
WiFi direct is : mwfd0
Actually you can change their names to yours.
Regards,
weidong
Hello @kbpanchal05 ,
Tell me the following information, please!
1. Linux kernel version.
2. your hardware platform.
3. logs after running ifconfig -a
4. logs after running lspci -k
5. your 9098 is a module designed by nxp partner or COB design on board?
Thanks!
Regards,
weidong
Any feedback on this ?
Kalpesh,
I believe you're getting the different interfaces loading for different functionality.
In your wifi_mod_para.conf, or on the command line for your insmod command, you can add the argument:
drv_mode=1
And it will just set the device up for STA functionality, which should support scanning.
For different functionality you can use different bit settings.
Bit 0 : STA
Bit 1 : uAP
Bit 2 : WIFIDIRECT
These can be combined for different modes, for example
1 : STA
2 : uAP
3 : STA + uAP
7 : STA + uAP + WIFIDIRECT
The default drv_mode is 7.
I believe you can also change the different mode settings while the driver is loaded, as such:
echo drv_mode=1 > /proc/mwlan/adapterX/config // STA
echo drv_mode=2 > /proc/mwlan/adapterX/config // uAP
echo drv_mode=3 > /proc/mwlan/adapterX/config // STA+uAP
echo drv_mode=7 > /proc/mwlan/adapterX/config // STA+uAP+WIFIDIRECT
Hope this helps,
-ryan
Hi @kbpanchal05 ,
Replied to you yesterday.
Didn't you see my answer ?
check it, please!
Regards,
weidong
Hello weidong,
Thanks a lot for your reply.
Here is my conf and firmware on file system.
# ls -l /lib/firmware/nxp/*
/lib/firmware/nxp/pcie9098_wlan_v1.bin
/lib/firmware/nxp/pcieuart9098_combo_v1.bin
/lib/firmware/nxp/uart9098_bt_v1.bin
/lib/firmware/nxp/wifi_mod_para.conf
----------------------------------------------
PCIE9098_0 = {
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode=7
ps_mode=2
auto_ds=2
fw_name=nxp/pcieuart9098_combo_v1.bin
}
---------------------------------------------------------------------------------
----------------------------------
echo "Starting WiFi"
# Load WiFi driver
modprobe moal mod_para=nxp/wifi_mod_para.conf
# Reload wireless regulatory.db
iw reg reload;
# Default set to US to use 5G channels allowed in USA
iw reg set US
----------------------------------
Thanks,
Kalpesh
Hello @kbpanchal05 ,
9098 supports 2 MACs , in your wifi_mod_para.conf, there should be 2 9098 modes.
PCIE9098_0 = {
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode=7
ps_mode=2
auto_ds=2
fw_name=nxp/pcieuart9098_combo_v1.bin
}
PCIE9098_1 = {
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode=7
ps_mode=2
auto_ds=2
fw_name=nxp/pcieuart9098_combo_v1.bin
}
Actually if you don't specify sta_name/uap_name/wfd_name/ drv_mode in the config file, the follwing interfaces will be created by 9098 driver:
MAC0: mlan0 / uap0 / wfd0.
MAC1 : mmlan0 / muap0 / mwfd0.
BUT for your configration , the following interfaces will be created:
MAC0: mlan0 / uap0 / p2p0. ( This is WiFi 6 , 802.11ax)
MAC1 : mmlan0 / muap0 / p2p1. (This is WiF 5 , 802.11ac)
So after loading driver, if you run "ifconfig -a" , you will see above 6 interfaces of 9098 under linux.
So you should confirm if these interfaces are correct.
Then run the following commands to connect it to ROUTER or Access Point.
=====================
# wpa_passphrase SSID PASSWORD >> /etc/wpa_supplicant.conf
# wpa_supplicant -d -B -i mlan0 -c /etc/wpa_supplicant.conf -Dnl80211
=====================
In order to verify if 9098 can access internet, you can ping 8.8.8.8 .
Regards,
weidong
Hello weidong,
sorry for the delay in reply. And Thank you so much for your response.
After debugging further more I tried with two different configuration
Case 1: With wfd_name as wfd and mwfd
PCIE9098_0 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=2
auto_ds=2
drv_mode=7
wfd_name=wfd
sta_name=mlan
uap_name=uap
host_mlme=1
mac_addr=00:50:43:20:12:34
fw_name=nxp/pcieuart9098_combo_v1.bin
}
PCIE9098_1 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=2
auto_ds=2
drv_mode=7
wfd_name=mwfd
sta_name=mmlan
uap_name=muap
host_mlme=1
mac_addr=00:50:43:20:52:56
fw_name=nxp/pcieuart9098_combo_v1.bin
}
Following interfaces are available with ifconfig -a command output
MAC0: mlan0 / uap0 / wfd0.
MAC1 : mmlan0 / muap0 / mwfd0.
Case 2: With wfd_name as p2p in both MAC
PCIE9098_0 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=2
auto_ds=2
drv_mode=7
wfd_name=p2p
sta_name=mlan
uap_name=uap
host_mlme=1
mac_addr=00:50:43:20:12:34
fw_name=nxp/pcieuart9098_combo_v1.bin
}
PCIE9098_1 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=2
auto_ds=2
drv_mode=7
wfd_name=p2p
sta_name=mmlan
uap_name=muap
host_mlme=1
mac_addr=00:50:43:20:52:56
fw_name=nxp/pcieuart9098_combo_v1.bin
}
Following interfaces are available with ifconfig -a command output first time
MAC0: wlp5s0f0/ uap0 / p2p0.
MAC1 : wlp5s0f1 / muap0 / p2p1.
muap0: flags=4098<BROADCAST,MULTICAST> mtu 1500
p2p0: flags=4098<BROADCAST,MULTICAST> mtu 1500
p2p1: flags=4098<BROADCAST,MULTICAST> mtu 1500
uap0: flags=4098<BROADCAST,MULTICAST> mtu 1500
wlp5s0f0: flags=4098<BROADCAST,MULTICAST> mtu 1500
wlp5s0f1: flags=4098<BROADCAST,MULTICAST> mtu 1500
mlan0 and mmlan0 missing
- Reloaded driver and interfaces available with ifconfig -a command output second time
mlan0: flags=4098<BROADCAST,MULTICAST> mtu 1500
mmlan0: flags=4098<BROADCAST,MULTICAST> mtu 1500
muap0: flags=4098<BROADCAST,MULTICAST> mtu 1500
p2p0: flags=4098<BROADCAST,MULTICAST> mtu 1500
wlp5s0f0: flags=4098<BROADCAST,MULTICAST> mtu 1500
wlp5s0f1: flags=4098<BROADCAST,MULTICAST> mtu 1500
And also sometimes uap0/p2p1 is NOT created . So In that case I have to reload the driver.
What is the difference between p2p and wfd / mwfd for wfd_name ?
Why it's affecting uap0/maln0/mmlan0/p2p interface creations in Case-2 ?
Can I use Case-1 configuration for using WiFi-6 and WiFi-5 mode ?
Are MAC0 and MAC1 hard configured to WiFi 6 (802.11ax) and WiF 5 (802.11ac) respectively on 88W9098 ? How can we verify that using command line ?
Thanks,
Kalpesh
Hello NXP Team,
Could you please provide your feedback on this ?
Thanks,
Kalpesh