We are using JN5179, and try to add OTA support in JN-AN-1220.
in section 5.7.2.1 "Using Makefiles" mentioned to add "OTA=1 to build with OTA client". But the whole project contains no OTA related files and very few words of OTA. Only one line "#APP_CLUSTERS_OTA_SRC ?=1" can be found in each makefile under directory build.
Please check if this JN-AN-1220 v1002 release really contains OTA support or not? Looks to me is NOT.
Thanks!
Hi Benjamin,
Your local sales will be in touch with you for solve this issue.
Regards,
Mario