Hi,
I was trying to boot the NXP drone following the tutorial this week but I met an issue with the QGroundControl. The QGC can automatically detect the drone via USB but not the telemetry radio. I tried many methods but still no luck yet.
What I’ve done:
The green lights of both telemetry radios are steady green so there should be a stable link between them but it still didn’t work. So I write to you to see if you have any idea about how to solve the issue.
Thanks,
Hi,
Hope you are doing well. Have you tried this yet? Connection problems · QGroundControl User Guide
This could help to debug the problem.
If you have any question please let me know.
Best Regards,
Ricardo
Yes, I tried the troubleshooting before but no new device was detected in the console. the troubleshooting page said it should be the hardware issue but I also tried 4 different telemetry radios so I guess the radio module should be fine. could it be the connection issue between the radio and the FMU?
and one thing that comes to my mind that on the telemetry radio manual page they said there are 2 LEDs on the module: green indicates the connection status between two radio modules and red(which is actually orange) flashing indicates data transferring. but I noticed that the radio module on the PC side has 3 LEDs and there is a real red led next to the green one is blinking. I'm not sure what's the meaning of that and could that be the reason?
Thanks,
Hey, I am currently having the same problem that you had. Were you able to fix it and if so how?