Hello,
I am using an NCJ29D5 chip with a custom PCB design. I connect my MCU to the NCJ29D5 chip with the SPI bus. I want to initialize the NCJ29D5 chip as an initiator role. To make sure, I send loopback_config and loopback_start commands.
1) Loopback Config Command : uint8_t CFG_LOOPBACK_CMD[11] = {0x2E,0x30,0x00,0x07,0x02,0x12,0x01,0x90,0x01,0x00,0x00};
I got the expected response from NCJ29D5 after this command
2) Loopback Start Command: START_LOOPBACK_CMD[4] = {0x2E,0x31,0x00,0x00};
I got the restart notification from the NCJ29D5 chip when I sent the loopback start command.
#000011 [ 20.048 ] INFO: (UWBSPI.c:914) B 0 0x6e
#000012 [ 20.048 ] INFO: (UWBSPI.c:915) B 1 0x0
#000013 [ 20.048 ] INFO: (UWBSPI.c:916) B 2 0x0
#000014 [ 20.048 ] INFO: (UWBSPI.c:917) B 3 0x5
#000015 [ 20.048 ] INFO: (UWBSPI.c:918) B 4 0x80
#000016 [ 20.048 ] INFO: (UWBSPI.c:919) B 5 0x0
#000017 [ 20.048 ] INFO: (UWBSPI.c:920) B 6 0x0
#000018 [ 20.048 ] INFO: (UWBSPI.c:921) B 7 0x0
I couldn't figure out why NCJ29D5 restarts itself after loopback_start command.
Is there any solution that you can provide?
Hello,
Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device and I do not have the data as well for the same reason.
For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have a direct contact, please communicate with him/her.
Regards,
Ricardo