NCJ29D5 INT_N pin is usually active low. I do not get any interrupt when it wakes up.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NCJ29D5 INT_N pin is usually active low. I do not get any interrupt when it wakes up.

915 Views
ahmed_sadek
Contributor I

NCJ29D5 INT_N pin is usually active low. I do not get any interrupt when it wakes up.

0 Kudos
1 Reply

891 Views
nxf63973
NXP Employee
NXP Employee

Hello

 

I'm sorry for the inconvenience this might cause you, but as the information of the  NCJ29D5 is under NDA (Non-Disclosure Agreement) the information of it it's not public, and I'm not able to check and verify as I do not have the information due to the security levels when working with an automotive part such as this.

 

Could you please contact your local distributor for assistance with this device?

 

Regards,

Jose

0 Kudos