IAR 7.50 KW40Z_Connectivity_Software_1.0.1
I'm trying to use the OTAP client for a MKW30Z hw target.
In cloned project bluetooth_otap_client_att\framework\Bootloader\Bootloader_OTAP_Serial
There is a bin file for MKW40Z BootloaderOTAP_KW40Z4.bin
For the MKW30Z target the bootloader should be rebuilt or is safe to use the default one ?
Thank you.
Solved! Go to Solution.
Hi Lucian,
Yes, It is safe to use the MKW40Z BootloaderOTAP_KW40Z4.bin.
Just remember MKW30Z doesn't support 802.15.4
Best Regards
Mario
Hi Lucian,
Yes, It is safe to use the MKW40Z BootloaderOTAP_KW40Z4.bin.
Just remember MKW30Z doesn't support 802.15.4
Best Regards
Mario
Hello Mario,
If I want to implement some end of flash region for serial number, hardware version, user config stuff, calibration data (Temp, TSI, RTC ...) should I modify the boot loader not to flash the end region of flash ?
Thank you,
Lucian
Hi Lucian,
If in your application you reserve a specific that region, it should not be any problem. So, all the .srec that you want to transmit with OTAP will save correctly
But, The boot loader could be like a back up, it will check again if the .srec file and it will determine if the new firmware is limited the flash like you set before.
Best Regards,
Mario
On below MKW40Z160_cfg.h
/** Kinetis Flash memory size */
#define KINETIS_FLASH (160*1024)
If I want to use, let say, the last page with serial number, HW version, calibration data,etc... can I modify this:
#define KINETIS_FLASH (159*1024)
KW40Z_Connectivity_Software_1.0.1\ConnSw\framework\Bootloader\Bootloader_OTAP_Serial\Linker_cfg
BootloaderOTAP.icf
/******************* Map of Kinetis FLASH ***********************************
+---------------+
| |
| |
| Application |
| |
| |
+---------------+ - __region_BOOT_ROM_end__
| Bootloader |
+---------------+ - __region_BOOT_ROM_start__
*****************************************************************************/
/*- Defining Symbols -*/
define exported symbol __region_BOOT_ROM_start__ = 0x00000000;
define exported symbol __region_BOOT_ROM_end__ = (gRomSize_c / 32) - 1;
define symbol __region_RAM_start__ = 0x20000000;
define symbol __region_RAM_end__ = 0x20001fff; // limit to 8K
/*-Sizes-*/
define symbol __size_cstack__ = 0x1000;
define symbol __IntVectTable_start__ = __region_BOOT_ROM_start__;
define symbol __IntVectTable_end__ = __region_BOOT_ROM_start__ + 0x3F;
define exported symbol __BOOT_STACK_ADDRESS = __region_RAM_end__ - 7; //0x20007FF8;
define symbol __code_start__ = __IntVectTable_end__+1;
define symbol __FlashConfig_start__ = 0x00000400;
define symbol __FlashConfig_end__ = 0x0000040f;
define block CSTACK with alignment = 8, size = __size_cstack__ { };
/*** Memory Regions ***/
define memory mem with size = 4G;
define region ROM_region = mem:[from (__IntVectTable_end__ + 1) to (__FlashConfig_start__ - 1)] | [from (__FlashConfig_end__+1) to __region_BOOT_ROM_end__];
define region RAM_region = mem:[from __region_RAM_start__ to __region_RAM_end__];
define region IntVectTable_region = mem:[from __IntVectTable_start__ to __IntVectTable_end__];
define region FlashConfig_region = mem:[from __FlashConfig_start__ to __FlashConfig_end__];
/*** Initialization ***/
do not initialize { readwrite };
do not initialize { section .noinit };
initialize manually { section .data};
initialize manually { section .textrw };
initialize by copy { section .IntVectTable };
/*** Memory placements ***/
place at address mem:__code_start__ { readonly section .noinit };
place in ROM_region { readonly };
place in RAM_region { readwrite, block CSTACK};
place in IntVectTable_region {section IntVectTable};
place in FlashConfig_region { section FlashConfig };
KW40Z_Connectivity_Software_1.0.1\ConnSw\framework\Bootloader\Bootloader_OTAP_Serial\src\include\cfg
MKW40Z160_cfg.h
/*!
* Copyright (c) 2015, Freescale Semiconductor, Inc.
* All rights reserved.
*
* \file MKW40Z160.h
* This file contains configuration options for the above processor
*
* Redistribution and use in source and binary forms, with or without modification,
* are permitted provided that the following conditions are met:
*
* o Redistributions of source code must retain the above copyright notice, this list
* of conditions and the following disclaimer.
*
* o Redistributions in binary form must reproduce the above copyright notice, this
* list of conditions and the following disclaimer in the documentation and/or
* other materials provided with the distribution.
*
* o Neither the name of Freescale Semiconductor, Inc. nor the names of its
* contributors may be used to endorse or promote products derived from this
* software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
* ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
* WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR
* ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
* LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON
* ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
* SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/**************************************************/
/** USER SETTINGS OF KINETIS MCU */
/** Kinetis ARM Cortex-M4 model */
#ifndef _MK21D256_CFG_H
#define _MK21D256_CFG_H
#define KINETIS_MODEL KW40_48MHz
/* in the case of using USB VIRTUAL SERIAL LINK you must activate No break TRIM CHECKBOX in the master AN2295 PC Application */
/* the break impulse is replaced by using only 9 bits zero impulse */
// BREAK IMPULSE |START| |0| |0| |0| |0| |0| |0| |0| |0| |0| |0| STOP|
// ZERO IMPULSE |START| |0| |0| |0| |0| |0| |0| |0| |0| |0| |STOP|
#define BOOTLOADER_SHORT_TRIM 1
/** Kinetis Flash memory size */
#define KINETIS_FLASH (160*1024)
/** Bootloader flash protection */
#define BOOTLOADER_FLASH_PROTECTION 0
/** Boot timeout after POR (Power On Reset) for wait to connect Master **/
/** BOOT_WAITING_TIMEOUT * 10ms **/
#define BOOT_WAITING_TIMEOUT 100
/**************************************************/
/* Actual used UART module */
#define BOOT_UART_BASE UART1_BASE_PTR
#define BOOT_UART_SIM_SCG_REG SIM_SCGC4
#define BOOT_UART_SIM_SCG_MASK SIM_SCGC4_UART1_MASK
#define BOOT_BUS_CLOCK (32768 * 640)
/* Actual used UART module */
/* A range of UART baudrates is (9600 - 115200) */
//#define BOOT_UART_BAUD_RATE 9600
//#define BOOT_UART_BAUD_RATE 14400
//#define BOOT_UART_BAUD_RATE 19200
//#define BOOT_UART_BAUD_RATE 38400
#define BOOT_UART_BAUD_RATE 57600
//#define BOOT_UART_BAUD_RATE 76800
//#define BOOT_UART_BAUD_RATE 115200
//#define BOOT_UART_BAUD_RATE 128000
/** GPIO & UART pins initialization */
#define BOOT_UART_GPIO_PORT_RX PORTE_BASE_PTR
#define BOOT_UART_GPIO_PORT_TX PORTE_BASE_PTR
#define BOOT_UART_GPIO_PORT_SIM_SCG_REG SIM_SCGC5
#define BOOT_UART_GPIO_PORT_SIM_SCG_MASK SIM_SCGC5_PORTE_MASK
/* setting of multiplexer for UART alternative of pin */
#define BOOT_PIN_UART_ALTERNATIVE 3
/* setting of multiplexer for GPIO alternative of pin */
#define BOOT_PIN_GPIO_ALTERNATIVE 1
#define BOOT_UART_GPIO_PIN_RX 1
#define BOOT_UART_GPIO_PIN_TX 0
/**************************************************/
/* Actual used PIN reset setting */
#define BOOT_PIN_ENABLE_SIM_SCG_REG SIM_SCGC5
#define BOOT_PIN_ENABLE_SIM_SCG_MASK SIM_SCGC5_PORTC_MASK
#define BOOT_PIN_ENABLE_PORT_BASE PORTC_BASE_PTR
#define BOOT_PIN_ENABLE_GPIO_BASE PTC_BASE_PTR
#define BOOT_PIN_ENABLE_NUM 4
/* CRC module clock gating info */
#define BOOT_CRC_SIM_SCG_REG SIM_SCGC6
#define BOOT_CRC_SIM_SCG_MASK SIM_SCGC6_CRC_MASK
/**************************************************/
/** BOOTLOADER FEATURES SETTINGS */
#define BOOTLOADER_ENABLE_READ_CMD 1
#define BOOTLOADER_INT_WATCHDOG 0
#define BOOTLOADER_ENABLE_VERIFY 1
#define BOOTLOADER_CRC_ENABLE 1
#define BOOTLOADER_AUTO_TRIMMING 1
#define BOOTLOADER_PIN_ENABLE 0
/**************************************************/
/** CALIBRATION OF BOOTLOADER TRIM SETTINGS */
#define BOOT_CALIBRATION_GPIO_BASE PTE_BASE_PTR
/******************************************************************************
*
*
* Advanced detail settings for non standard settings
*
*
******************************************************************************/
#define VECTOR_TABLE_SIZE (48*4)
/* Flash block count of this MCU */
#define FLASH_BLOCK_CNT 1
/* Start address of interrupt vector table */
#define INTERRUPT_VECTORS 0x0000
/* Start address of relocated interrutp vector table */
#define RELOCATED_VECTORS 0x4000
/* Flash start address */
#define USER_FLASH_START RELOCATED_VECTORS
/* Flash end address */
//#define USER_FLASH_END 0x0003FFFF
/* Flash2 start address */
//#define USER_FLASH_START_2 0x00040000
/* Flash2 end address */
//#define USER_FLASH_END_2 0x0005FFFF
/* Size of write block */
#define FLASH_WRITE_PAGE 128
/* Size of erase block */
#define FLASH_ERASE_PAGE 1024
/* Maximal length of ID_STRING */
//#define ID_STRING_MAX 5
/* Description string */
#define KINETIS_MODEL_STR "KL46"
#define FLASH_INIT_FLASH_CLOCK { SIM_SCGC6 |= SIM_SCGC6_FTF_MASK; }
#define FLASH_BASE_PTR FTFA_BASE_PTR
#define FLASH_FSTAT FTFA_FSTAT
#define FLASH_FSTAT_CCIF_MASK FTFA_FSTAT_CCIF_MASK
#define FLASH_FSTAT_ACCERR_MASK FTFA_FSTAT_ACCERR_MASK
#define FLASH_FSTAT_FPVIOL_MASK FTFA_FSTAT_FPVIOL_MASK
#define FLASH_FSTAT_RDCOLERR_MASK FTFA_FSTAT_RDCOLERR_MASK
#define FLASH_FSTAT_MGSTAT0_MASK FTFA_FSTAT_MGSTAT0_MASK
#endif//MK21D5_CFG_H