MKW30Z OTAP test on Kinetis BLE Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKW30Z OTAP test on Kinetis BLE Toolbox

926 Views
lucianfiran
Contributor V

IAR 7.50  KW40Z_Connectivity_Software_1.0.1 KSDK_1.3.0

To test the OTAP program, after connecting you can see device info profile by pressing the :smileyalert: (exclamation mark in circle)

and open a file.

What type of file do I need to open to upload ?

pastedImage_2.png

Got C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\tools\ble_otap

pastedImage_2.png

Should I use the srec file or the img file after using the python script or bat command ?

Inline image

O can I use bin files ?

C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\tools\binaries

IAR 7.5 output file selection:

pastedImage_5.png

- srec

- img

- bin

- other

Thank you,

Lucian.

Tags (5)
2 Replies

519 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Lucian,

Did you take a look for the next DOC? The KW40 only supports .srec files.

https://community.nxp.com/docs/DOC-332325 

Let me know if you have the same problem.

Best Regards,

Mario

519 Views
lucianfiran
Contributor V

srec files seems to be valid.

But what can be the reason that the update don't start ?

pastedImage_1.png

Thank you,

Lucian

0 Kudos