MKW22D and MKW24D difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKW22D and MKW24D difference

1,284 Views
bimal
Contributor III

Hi,

I wanted to know the difeerences between MKW22D and MKW24D,

As it seems like both are pin compatible, both has equal Flash and RAM. Is there any major difference between them?

Labels (3)
0 Kudos
3 Replies

817 Views
EarlOrlando
Senior Contributor II

Hello Bimalsinh,

The differences are listed in the table 2.1 "Ordering Information" in the MKW2xD Reference Manual​.

kw.jpg

Best regards,

Earl.

817 Views
bimal
Contributor III

Hi Earl,

Thanks for your feedback,

It seems like MKW24 supports Smart Energy 2.0, where as MKW22 doesn't. I am assuming that is the difference between them, otherwise they are same in Hardware architecture with pin-compatible.

I have one other question that, Does smart energy 2.0 requires any specific Hardware feature(like hardware stack support, IP stack) which is not there in MKW22?

0 Kudos

817 Views
jc_pacheco
NXP Employee
NXP Employee

SE2.0 relies on the SW stack, no hardware dependency. Only supported on MKW24.

0 Kudos