Hello,
I have done to setup the driver(as USER Guide) and have tested (output as below) but I get the error.
How can I fix it?
Name: Dut labtool
Version: 1.0.0.11
Date: Dec 18 2020 (09:52:40)
Note:
1. =========WiFi tool=============
2. =========BT tool=============
Enter CMD 99 to Exit
Enter option: 1
Name: DutApiClass
Interface: EtherNet
Version: 1.0.0.11
Date: Dec 18 2020 (09:51:38)
Note:
C:\Users\User\Desktop\新規WIFIモジュール資料\MFG-W8978-MF-WIFI-BT-BRG-FC-VS2013-1.0.0.11-16.80.10.p132\bin\release\labtool\setup.ini
Dut's IP 192.168.1.100:9930
Host's IP 192.168.1.10:9931
DutIf_UdpIp::delay 0
DutIf_UdpIp::vg_IfSpy 0
TCP connecting...
DutIf_InitConnection: 0x00000000
--------------------------------------------------------
W89xx (802.11a/g/b/n/ac) TEST MENU
--------------------------------------------------------
Enter option: 88
DLL Version : 1.0.0.11
LabTool Version: 1.0.0.11
DutIf_GetFWVersion: 0xFFFFFFF9
SOC OR Version: 0.0 Customer ID: 0
RF OR Version: 0.0 Customer ID: 0
Enter option: 9
DutIf_GetTxAntenna : Antenna 0 0xFFFFFFF9
Enter option: 13
DutIf_GetTxDataRate: 0xFFFFFFF9
Enter option: 11
DutIf_GetRfChannel: 0xFFFFFFF9
RF Channel: 0 (0.0 MHz)
Enter option: 45
Feature is not supported in CONF file mode
Enter option: 111
DutIf_GetChannelBw: 0xFFFFFFF9
Channel Bw: 0
Enter option: 198
DutIf_WlanRSSI_Cal_Start: 0xFFFFFFF9
Enter option:
Dear @Ta_exa
Could you clarify if that support request is concerning IW416 (88W8978) or 88W8997 ?
Regards,
Olivier