Kinetis Pin Compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Pin Compatibility

Jump to solution
1,312 Views
atillametetured
Contributor V

Hello,

I am at the edge of selecting our ZigBee and Thread Device and am torn between MKW21D512, MKW22D512 and MKW24D512. Are these devices pin compatible. What I think is MKW21D512 is not compatible with 22D and 24D. Can someone confirm this? Also all devices share the same memory properties so I assume they all support ZigBee and Thread simultaneously (I know only 24D supports SE 2.0 profile, I dont know the reason though, can someone also point out why?)

Thanks in advance for help,

Best Regards,

Mete

Labels (2)
Tags (4)
0 Kudos
1 Solution
1,002 Views
EarlOrlando
Senior Contributor II

Hello Mete,

As you can see MKW2xD Reference Manual​, these three devices have differences only in the Smart Energy, USB and FlexMemory support.

MKW2XD.jpg

Best regards,

Earl Ramírez.

View solution in original post

1 Reply
1,003 Views
EarlOrlando
Senior Contributor II

Hello Mete,

As you can see MKW2xD Reference Manual​, these three devices have differences only in the Smart Energy, USB and FlexMemory support.

MKW2XD.jpg

Best regards,

Earl Ramírez.