Kinetis (KW35/38/KW45 & K32W1/MCX W71) Power Profile Tools (including Localization)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis (KW35/38/KW45 & K32W1/MCX W71) Power Profile Tools (including Localization)

跳至解决方案
15,610 次查看
christophe_menard
NXP Employee
NXP Employee

This page is dedicated to the Kinetis (KW35/KW38/KW45) and MCX W7x (MCX W71) Power Profile Tools.

It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery life time of your solution.

This page content 5 dedicated power profile tool for:

  1. Bluetooth LE for the KW35/KW38/KW45 products in standalone (Automotive).
  2. Bluetooth LE for the MCX W71 product in standalone (IIoT).
  3. 802.15.4 Matter ICD SIT & LIT and ZED for the MCX W71 product in standalone (IIoT).
  4. SmartFob application (BLE/KW45; UWB Ranger4; SE; motion sensor) (Automotive)
  5. Localisation application (CCCv4) (Automotive & IIoT)

 

1. KW35/KW38/KW45 Bluetooth LE Power profiles

christophe_menard_0-1728316470360.png

 

This tool includes 3 different use cases to get a rough estimation of the Anchor and Keyfob/Smartphone power consumptions:

   1- CCC mobile phone connected to the car and exchange packets to unlock the door of the car

   2- SCA Keyfob connected to the car and exchange packets continuously

   3- CCC Smartphone connected to the car and exchange packets continuously : 2 row modes

christophe_menard_6-1710781541302.png

2. IIoT MCX W71 Bluetooth LE Power profile

christophe_menard_0-1719240520534.png

 

3. 802.15.4 Matter ICD SIT & LIT and ZED MCX W71 Power profile

christophe_menard_0-1732722849046.png

4. Smartfob Power profile

christophe_menard_4-1710780975560.png

 

5. CCCv4 localization power profile

2 automotive applications example are available in the KW45 SDK:

...\kw45b41zevk\wireless_examples\bluetooth\digital_key_car_anchor_cs

...\kw45b41zevk\wireless_examples\bluetooth\digital_key_device_cs

christophe_menard_0-1727875028159.png

 

2 IIoT applications example are available in the MCX W71 SDK:

...\MCX W71\boards\k32w148evk\wireless_examples\bluetooth\loc_reader

...\MCX W71\boards\k32w148evk\wireless_examples\bluetooth\loc_user_device

 

Please, find this important link to build a PCB using a KW45 or MCX W71 and all concerning the radio performances and radio certification (CE/FCC/IC):

The best way to build a PCB using a KW45 (car acce... - NXP Community

 

For Power and Low Power Application Notes please see product pages. Here are some direct links for your convenience:

MCXW71 - Power Management Hardware

MCX W71 Bluetooth LE Power Consumption Analysis

KW45/K32W148 - Power Management Hardware

Kinetis KW45 and K32W1 Bluetooth LE Power Consumption Analysis

 

0 项奖励
回复
1 解答
13,871 次查看
christophe_menard
NXP Employee
NXP Employee

Hi Everett,

The password is in place to avoid changes or competitor benchmarks in too much details.

Sorry for the inconvenient but it can't be.

在原帖中查看解决方案

2 回复数
13,872 次查看
christophe_menard
NXP Employee
NXP Employee

Hi Everett,

The password is in place to avoid changes or competitor benchmarks in too much details.

Sorry for the inconvenient but it can't be.

13,903 次查看
EverettRao
NXP Employee
NXP Employee

Hi  christophe_menard,

@christophe_menard  Could you provide the password of Sheet protection, thanks very much.

EverettRao_0-1729134009121.png

 

0 项奖励
回复