KW41Z - concurrent operation of stack's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z - concurrent operation of stack's

692 Views
adrian_chmiel
Contributor III

Hi,

I found information, that KW41Z support concurrent operation of wireless comunication.

Is there documentation on how to do this?

In MCUexpresso middleware selection does not work when I create project (middleware  section is empty, SDK have included all stacks).

So I should takeoff stak from SDK manualy and them run it in MSUexpresso project?

0 Kudos
1 Reply

631 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Adrian, I hope you're doing well!

 

Are you referring to Wireless Protocol Coexistence? If this is the case, the SDK examples offers example projects showing hybrid operation of the BLE and either ZigBee, 802.15.4 or Thread Stacks.

 

These example and base projects can be found in the following folder of the SDK package:

 

<…\SDK_SDK_2.2.1_FRDM-KW41Z\boards\frdmkw41z\wireless_examples\hybrid>

 

Please let me know if that's not what you meant, or if you need any more information.

 

Best regards,

Sebastian

0 Kudos