KW41Z Thread

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z Thread

1,588 Views
sensenthuran
Contributor IV

Can the  Home Kit sensors connect to KW41Z based border router network? , if so, how we should configure the KW41Z router to commission? 

example sensors 

Eve Door & Window - Apple HomeKit

https://www.amazon.ca/Eve-Door-Window-Automatically-Notifications/dp/B08BDM47S2?ref_=ast_sto_dp&th=1...

 

Wemo Smart Plug with Thread 

https://www.amazon.com/HomeKit-Enabled-Automation-Compatible-Controller/dp/B09T4S3QKC/ref=sr_1_3?cri...

 

Labels (2)
0 Kudos
3 Replies

1,346 Views
patrick_pan
NXP Employee
NXP Employee

Hi, Sen

Theoretically the KW41 Thread BR is not HomeKit device, so it will not accept Homekit Accessory to join its network since the commissioning and pairing stages of Homekit Accessory requires either HW or SW MFI certified messages like credential / provisioning data be exchanged between Homekit Controller and Accessory. The KW41 Thread BR most probably will not provide these mandatory Homekit required information so Homekit Accessory wouldn't join it successfully.

 

B.R

Patrick

 

 

1,337 Views
sensenthuran
Contributor IV

Thanks @patrick_pan 

We already tested KW41Z Thread Border gateway with Eval board sensors.

Would your recommend any commercial Thread sensors that can connect to NXP KW41Z Thread Border Gateway?

 

0 Kudos

1,430 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Please help us checking this page with the current support of HOMEKIT , there you can also find some details on how to seek for more details as well.

 

Regards,