Hi
I´m developing a project that works with the MCU KW41Z on MCUXpresso IDE.
I´m new at MCUXpresso (i used to work on Kinetis Design Studio with other microcontroler: kl27z256). at KDS, i used to work with processor expert, and had all the libreries for lpuart comunication.
On MCUXpresso, i understand that for mi microcontroler (KW41Z), I cant use the peripheral config tool .
im trying with the fsl_lpuart.h library, but its not working.
Could anyone tell me the best way to implement lpuart comunications in my project.
Thanks
Jose
Hi,
You can use the example. Click 'import SDK examples'. Choose your board. Then you can import the
lpuart example.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------