KW40Z Connectivity Software hidden software switches

cancel
Showing results for 
Search instead for 
Did you mean: 

KW40Z Connectivity Software hidden software switches

308 Views
lucianfiran
Contributor V

IAR 7.50;  KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0)

As some module get pre-compiled in the framework like Bluetooth stack, there is a list of necessary, must-have predefines that influence these modules ?

Are some especially defines, design for building with MKW30Z ?

Tags (3)
0 Kudos
2 Replies

103 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Lucian,

Only the files that are in the Bluetooth/host are pre-compiled, so if you for any reason change some defines, the changes that you did, will be ignored. That values work as a reference code.

Regards,

Mario

0 Kudos

103 Views
lucianfiran
Contributor V

what about:

/*! *********************************************************************************
 *     bluetooth - BLE Stack Configuration
 ********************************************************************************** */

  /*! *********************************************************************************
   *     controller
   ********************************************************************************** */
  /*! *********************************************************************************
   *     hci_transport
   ********************************************************************************** */
    /* hci_transport.h*/
      #define APP_SERIAL_INTERFACE_TYPE      (gSerialMgrNone_c)
      #define APP_SERIAL_INTERFACE_INSTANCE  (0)                 
                 
  /*! *********************************************************************************
   *     host
   ********************************************************************************** */
    /* ble_general.h */
      /* Range  0x0006 0xFFFF  default 40 <> 50ms */
      #define gcConnectionIntervalMinDefault_c            (40)
      /* Range  0x0000 0xFFFF  default 160 <> 200ms */
      #define gcConnectionIntervalMaxDefault_c            (160)
      #define gcConnectionSlaveLatencyDefault_c           (0)
      /*! Time = N * 10 ms */
      /* Range    default 2000 <> 20sec */                  
      #define gcConnectionSupervisionTimeoutDefault_c     (2000)
      /*! Time = N * 0.625 ms */                 
      #define gcConnectionEventMinDefault_c               (0)
      /*! Time = N * 0.625 ms */                 
      #define gcConnectionEventMaxDefault_c               (0)                 
                 
  /*! *********************************************************************************
   *     profiles
   ********************************************************************************** */
              
  /*! *********************************************************************************
   *     app common
   ********************************************************************************** */
    /* ble_controller_task.c */                              
      #define BD_ADDR             0x13,0x00,0x00,0x9F,0x04,0x00

    /* ble_controller_task_config.h */
      /* Range   default 900 */
      #define gControllerTaskStackSize_c 900
      /* Range   default 1 */           
      #define gControllerTaskPriority_c 1  

    /* ble_host_task_config.h */  
      /* Range   default 1300 */
      #define gHost_TaskStackSize_c 1300  
      /* Range   default 5 */
      #define gHost_TaskPriority_c     5
      /* Range   default 800 */
      #define gL2ca_TaskStackSize_c  800
      /* Range   default 4 */
      #define gL2ca_TaskPriority_c     4
      /* Range time <= 10msec  default  0x08 <-> 5msec */               
      #define mcAdvertisingPacketInterval_c     0x08                     
      /* Range  0x01 - 0x07  default  0x07 */      
      #define mcScanChannelMap_c                0x07
      /* Range  0x01 - 0x07  default  0x07 */                    
      #define mcInitiatorChannelMap_c           0x07
      #define mcOffsetToFirstInstant_c          0xFFFF  
      /* Default Tx Power on the advertising channel.  */
      /* Range  0-15  default  5  */
      #define mAdvertisingDefaultTxPower_c      5  
      /* Default Tx Power on the connection channel.  */
      /* Range  0-15  default  5  */                  
      #define mConnectionDefaultTxPower_c       5  

0 Kudos