Hello,
Request your kindly help to solve the hard fault issue about the BLE central mode.
Hardware: KW38 EVB
SDK: SDK_2_x_FRDM-KW38 2.6.13.201911251446
I use the SDK example - "wireless_uart_bm" as my demo application.
For continuously scanning at central mode, I remove "Gap_StopScanning()" in function "ScanningTimerCallback".
When demo applicaiton running on the EVB.
Press 'PB1" to start the scanning procedure. (Don't need to connect any peripheral device).
After a couple of time, EVB is crashed and MCUXpresso IDE stopped and show the "Active faults" message.
The following is my screen capture.
How to solve this issue?
Thanks.
Tim