Hi,
I am working on using CAN bus to upgrade image on kw36 by following the attached document's process.
I generate the bleota file which is attached below by using NXP test tool 12 according to
Chapter 3: Image obtaining
After IoT toolbox app connected with CAN Node A v1 board successfully, I press open button to load the bleota file but which is failed and the error can be seen in the picture below.
How to upload a bleota file ?
Thank you for helping!
Hi @Lincoln,
What is the file that you trying to send over the IoT Toolbox?
The app only supports bin, srec and s19 files.
Regards,
Mario
Hi @mario_castaneda,
I am sorry that I didn't attach successfully the document and file I've mentioned in previous post.
According to image obtaining procedure in the attached doc, I obtain a .bleota file which can be found in file attached after following the process below.
Hi @Lincoln,
I am really sorry. I confirmed with the validation team. IoT Toolbox does not support .s19 file, only supports .srec and .bleota file. You can change the .s19 to .srec directly,then firmware can be updated successfully.
So, in this case, you could import the image into a srec file and the tool will create a correct .bleota file.
Please let me know your findings.
Regards,
Mario
Hi @mario_castaneda,
After my testing, it turns out that IoT Toolbox app does support .s19 file but not support .bleota file.
Every time I upload .bleota file to the app, it would show "unknown error" as I already mentioned.
As for this case, using NXP Test Tool 12 to modify image id to 0x000A is required for CAN bus image upgrading process. However the image would be saved as .bleota file which cannot be loaded into IoT Toolbox app for OTA purpose.
What is the solution for this case?
Hi @Lincoln,
I tested by my side using the bleota file and it works.
Is it possible that you could share the bleota file?
Regards,
Mario
Hi @Lincoln,
I tested your bleota file, and it works. The app detects a valid file.
What is the version that you have installed? My version is 5.4.1
The process that I am following is:
Regards,
Mario
Hi @mario_castaneda,
It is still failed to work with the bleota file.
I cannot see where goes wrong.
Here is my IoT tool version, which seems different from yours?
And I follow the process below:
Note:
I am working with FRDM-KW36 SDK 2.2.9
Is there anything I missing?
Or an alternative can be implemented?
Thank you.
Hi @Lincoln,
Is it possible that you could update the SDK version to the last one?
The current version that we have is 2.6.14.
It is a strange issue, but is it possible that you could uninstall the IoTToolbox and install it again?
Please let me know your findings.
Regards,
Mario