KW36: Why Write Response not sent for Write request?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36: Why Write Response not sent for Write request?

580 Views
skalyan2
Contributor IV

Hi,

I am facing a issue in KW36 in sending Write response command. In my case is that my mobile app is trying to enable Client Characteristic Configuration Descriptor(CCCD) for a characteristic in my gattdb, but when the app sends Write Request for the writing the CCCD, the NXP stack doesn't send the Write Response sometimes for that.

Because of this my app disconnects from the KW36, 30 seconds after the Write Request is sent(I assume this is because of supervision timeout in phone/app)

I have attached the airtrace in which I have bookmarked my issue.

Regards,

Sai Kalyana Raman

Labels (3)
0 Kudos
1 Reply

472 Views
xing_chang
NXP Employee
NXP Employee

Hi skalyan2@visteon.com‌,

Your HID device is mouse or keyboard, maybe the operating system took over the control of HID, so you can't operate it.

0 Kudos