KW36无法在Buck Mode状态下下载程序

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36无法在Buck Mode状态下下载程序

1,053 Views
chakan122
Contributor I

工程师,你好!

        我设计的KW36的电路板在Buck Mode(auto start)模式下无法使用SEGGER J-Link 下载程序。但通过短接J27,使VDD_BRD变为3.3V,才可以调试下载程序。下载好程序的KW36可以工作在Buck Mode(auto start),但仍然无法在该模式下下载程序。我的电路与 【FREEDOM KW36 Bluetooth Smart/Generic FSK】基本一致。

kw36power.jpg

kw36.jpg

红叉部分未焊接。外围元件基本没焊。

错误提示如下,几乎和未连接到目标板的状态一样。

使用官方MCUXpresso IDE v11.1.1_3241编译调试。

error main.jpg

event details.jpg

以上

谢谢!

Labels (1)
0 Kudos
1 Reply

1,003 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

Could you please take a look at the DCDC Power Management document for the KW4x/KW3xA/Z/KW2xZ series of MCUs?

 

It provides detailed information on the different possible configurations for the DC-DC in these MCUs.

 

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 Kudos