KW24D512 ZigBee + KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW24D512 ZigBee + KDS

886 Views
daviddanaj
Contributor I

Hi.

Is it possible to develop code for FRDM-KW24D512 using ZigBee stack in KDS and without OS?

So far I have tried:

  1. Freescale BeeKit (most promising so far)
    I used 'User Defined Target' when creating new project in BeeKit because there is only TWR or USB option (not FRDM)
    After exporting solution from BeeKit and importing into KDS there is a message "Nothing to build for project xxx" when I try to build it. 
  2. BeeStack 5.0
    In examples in BeeStack 5.0, I have found only projects for FreeRTOS and MQX (no bare-metal). And also only for IAR.
  3. MKW2xD_MCR20A Connectivity Software
    There are examples only for SMAC and IEEE 802.15.4. There are not examples for ZigBee.

Thank you for any suggestions.

KDS version: 3.2.0

Labels (1)
0 Kudos
1 Reply

566 Views
jc_pacheco
NXP Employee
NXP Employee

Hello David,

BeeStack (ZigBee) will no longer be supported on future releases. This also means that there will be no support on KDS for Connectivity Software on KW2xD. Last build is OS dependent and libraries are compiled in IAR so it's required for development.

MKW41Z Connectivity Software covers: BLE, Thread, GENFSK, IEEE802.15.4 and SMAC in case you are interested on those other Wireless Connectivity stacks.

0 Kudos