1. Update with "DK6 Production Flash Programmer".
I know that when using LPC-Link2 USB connection can not reach 1M baud rate, what is the default speed?
What is the highest speed that can be set in LPC-Link2?
2. If the SOC uses UART0 to connect to K32W,
Can K32W receive 1M baud rate?
Does RTS/CTS need to be connected?
I tried using "default baud rate" and "-P 115200", but it took about the same time for download.
"which speed are you referring to" on LPC-Link2 ?
Hello,
Could you please try setting the verbosity in a higher level so we can verify about the boudrate ?
Regards,
Estephania
Hello,
Do you mean with the SWD programming ? Or which speed are you referring to ?
The questions 2 was already solved in https://community.nxp.com/thread/535671
Regards,
Estephania