If the SOC(Wifi module) is connected to K32W,
can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?
Thank you for your reply, let me know that 1M uart speed can be achieved without CTS/RTS.
Hello,
it is good that this is clear now.
Regards,
Estephania
Hello,
The device can support up to 1M speed , the usage of the CTS and RTS are mostly used in application level and is up to the customers if they use it or not.
In this case the flash programmer can work without CTS and RTS, you can check more information about this in the Production Flash Programmer Guide.
Regards,
Estephania