K32W ISP mode

cancel
Showing results for 
Search instead for 
Did you mean: 

K32W ISP mode

93 Views
Contributor V

If the SOC(Wifi module) is connected to K32W,

can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?

Labels (1)
  • KW

0 Kudos
3 Replies

7 Views
Contributor V

Thank you for your reply, let me know that 1M uart speed can be achieved without CTS/RTS.

0 Kudos

7 Views
NXP TechSupport
NXP TechSupport

Hello,

it is good that this is clear now.

Regards,
Estephania

0 Kudos

7 Views
NXP TechSupport
NXP TechSupport

Hello,

The device can support up to 1M speed , the usage of the CTS and RTS are mostly used in application level and is up to the customers if they use it or not.

In this case the flash programmer can work without CTS and RTS, you can check more information about this in the Production Flash Programmer Guide.

Regards,
Estephania

0 Kudos