K32W CMET operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W CMET operation

999 Views
danieltseng
Contributor V

I read jn-an-1242,May I ask how to use CMET in pairs?

pastedImage_1.png

Labels (1)
  • KW

0 Kudos
5 Replies

868 Views
danieltseng
Contributor V

I have studied the content you mentioned before, but I still don’t know how to choose these two functions to achieve these functions.

The content does not provide what to do. For example: KW41 has a very detailed description.

This is my first contact with CMET (different from KW41 GenFSK), so I am not familiar with it, so please give me some guidance.

pastedImage_1.png

0 Kudos

868 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel,

 

Could you please take a look at chapter 3 of the following application note?:

 

K32W RF system evaluation report for Bluetooth LE and 802.15.4 applications

 

It provides a more in-depth explanation of the test modes for this device.

 

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 Kudos

868 Views
danieltseng
Contributor V

What I want to know is how to use (a) ~ (m) items  in pairs?

Example: (a) as TX corresponds to (c) as RX

Please provide other options that can be combined with each other?

a,b --> c
d --> ?
f  --> ?
g --> ?
h --> ?
i  --> ?
j  --> ?
k --> ?
l  --> ?
m --> ?

There is no explanation in the document( JN-AN-1242) about how to combine the two options.

0 Kudos

868 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel,

 

The descriptions for each of the Test Modes in the CMET document contain information on the mode they'll be setting the device to, like for example the Receive Packets Test:

 pastedImage_1.png

Or the LQI test:

pastedImage_3.png

The combinations have to be done with a transmitter and a receiver mode, while some of the other modes like the Connectionless Packet Error Rate Test need both devices to be configured in the same test mode, but as a Slave or Master:

pastedImage_4.png

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 Kudos

868 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

To use the CMET Application Note in pairs, two K32W devices must be programmed with this firmware, and then, one of the devices should be configured in the Transmit Packets Test Mode, while the other device should be configured in one of the Receive Packets modes, like the Generic Receive Packets Test, the LQI Test, or the RX-to-TX Turnaround Test.

 

Most of the Tests require at least two devices to work, one in Transmit, and one in Receive mode.

 

Please let me know if you need specific information about one of the test modes.

 

Best regards,

Sebastian

0 Kudos