Hi All,
The chip I use is JN5189, the SDK version I use is SDK2.6.2_JN5189DK6, and the routine I use is Zigbee_ed_rx_off.
The default setting of this routine can realize the timing wake-up of the device. In addition, I hope to realize that when the module is sleeping, press the wake-up button to immediately wake up the device, and when the wake-up button is released, the module will continue to sleep in accordance with the sleep cycle.
How to realize this function?
BR,
Viki
Hi @Viki,
I hope you are doing great.
I recommend looking at the JN-AN-1246 that could help you with the implementation of the button and also the routines that the code implements.
Regards,
Mario