With JN5179, we hope to perform enrolment to IASZone device. We take Device (JN-AN-1218-Zigbee-3-0-Light-Bulb-v1002,DimmableLight), and added IASzone cluster. Try on Coordinator (JN-AN-1216-Zigbee-3-0-IoT-ControlBridge) with ZGWUI tool, but failed.
We followed "Section 36 of JN-UG-3115", and try to accomplish "36.3.2 Auto-Enroll-Response". The 2nd item is "Write Attribute command" with IEEE address (8-byte). But "data" field of ZGWUI can accept single hex data only. Below are the logs. Please check and comment. Is there a way that we can accomplish the enrollment task using ZGWUI?
09:28:16.189 -> 01 02 11 02 10 02 10 02 1E E6 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 03
09:28:16.301 <- 01 80 00 00 04 83 00 06 01 00 03
09:28:16.371 <- 01 81 00 00 14 94 06 6A 81 01 05 00 00 10 00 F0 00 08 00 00 00 00 00 00 00 00 03
Type: 0x8000 (Status)
Length: 4
Status: 0x00 (Success)
SQN: 0x06
Message: _
Type: 0x8100 (Read Attrib Response)
SQN: 0x06
Src Addr: 0x6A81
EndPoint: 0x01
Status: 0x00
Cluster ID: 0x0500 (Security & Safety: IAS Zone)
Attribute ID: 0x0010
Attribute Size: 0x0008
Attribute Type: 0xF0 (IEEE Address)
Attribute Data: 00:00:00:00:00:00:00:00 //(IEEE address after reset)
<2>[Write Attrib] with (Type:E_ZCL_IEEE_ADDR = 0xf0, Data=0x38 //1-byte, ZGWUI required(or err)
>Got: (Write Attrib Response) with error!
09:28:33.165 -> 01 02 11 10 02 10 10 20 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 F0 38 03
09:28:33.309 <- 01 80 00 00 04 92 00 07 01 10 03
09:28:33.401 <- 01 81 10 00 0C 12 07 6A 81 01 05 00 7F 38 20 00 00 00 03
Type: 0x8000 (Status)
Length: 4
Status: 0x00 (Success)
SQN: 0x07
Message: __
Type: 0x8110 (Write Attrib Response)
SQN: 0x07
Src Addr: 0x6A81
Src Ep: 0x01
Cluster ID: 0x0500 (Security & Safety: IAS Zone)
Attribute ID: 0x7F38 // error why?
Attribute Size: 0x0000 // ??
Attribute Type: 0x00 (Unknown) // ??
Status: 0x20 // ??
09:28:40.796 -> 01 02 11 02 10 02 10 02 1E E6 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 03
09:28:40.933 <- 01 80 00 00 04 8D 00 08 01 00 03
09:28:42.551 <- 01 81 00 00 14 9A 08 6A 81 01 05 00 00 10 00 F0 00 08 38 38 38 38 38 38 38 38 03
Type: 0x8000 (Status)
Length: 4
Status: 0x00 (Success)
SQN: 0x08
Message: _
Type: 0x8100 (Read Attrib Response)
SQN: 0x08
Src Addr: 0x6A81
EndPoint: 0x01
Status: 0x00
Cluster ID: 0x0500 (Security & Safety: IAS Zone)
Attribute ID: 0x0010
Attribute Size: 0x0008
Attribute Type: 0xF0 (IEEE Address)
Attribute Data: 38:38:38:38:38:38:38:38 // seems the 1st byte has been changed
<4.TBD>[Write Attrib] with Data=00:15:8D :00:00:E0:7A:3E //8-byte,ZGWUI is to be revised
Benjamin
Hi Benjamin,
A local sales will be in touch with you for solve this issue.
Regards,
Mario
Hi Mario,
I am also having the same query. I am having one Door Sensor (IAS Zone Device). I want to enroll it using IEEE address of control bridge app (running on JN5179 USB dongle) by write attribute command from ZGWUI. But the tool is not allowing me to write 8 bytes. Can you please help me here to get the solution?
Thanks,
Vivek