JN5169+PA距离问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5169+PA距离问题

1,379 Views
dezhuangqiu
Contributor II

我们现在的一个项目用的是JN5169,协调器是是1216没有修改,路由器用的是1218修改的,但是遇到几个问题:

1、距离,协调器和路由器点对点传输只有8米左右,我们要求30米,有人建议加PA,但是程序不会改;

2、我们现在的设备有灯,插座、窗帘等,都是开关量,用的是同一个程序,协调器怎么识别不同的设备类型?

PA.png

Tags (1)
0 Kudos
Reply
2 Replies

1,135 Views
dezhuangqiu
Contributor II

5169.png

这是哦=我没加PA 的图纸,传输距离只有8米左右,请问这是哪里的问题?

加PA之后程序都是要修改的,因为要使能PA芯片,这个不知道怎么修改?

0 Kudos
Reply

1,135 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dezhuang Qiu,

What is the JN5169 module or JN5169 that you are working on?

By default, all the examples, that we provide, enable the high power module depending on the JN device.

Regards,

Mario

0 Kudos
Reply