JN5168 - Wake up on 'either' rising or falling edge

cancel
Showing results for 
Search instead for 
Did you mean: 

JN5168 - Wake up on 'either' rising or falling edge

259 Views
meg1
Contributor I

Hello there! 

Im doing my first JN5168 project, and first JenOS project ever (never used any nxp processors) 

Im trying to figure out 2 things.

1, I have a toggle switch that I want to use to wake up the MCU whenever is toggled (rising or falling) 

      Is the only was to do this to connect the switch to 2 diffrent inputs and have one vAHI_DioWakeEdge() for rising and one for falling?

2. What happens upon a wake called by a DIO? after enabling vAHI_DioWakeEnable(), which function will be executed upon the wake up? I want to use the wake up kinda like an interrupt, where it runs one specific function?

Thanks for the beginner help!

Labels (3)
Tags (3)
0 Kudos
1 Reply

170 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Martin,

Could you please look at the JN-AN-1189 Zigbee HA Demo? You will find the APP_bButtonInitialise function that provides initialization of the buttons, pull-up, edge detections, interrupts.

ZigBee Home Automation | NXP 

Regards,

Mario

0 Kudos