hi,
in my application, i used the JN5168-001-MXX, and there was only one Co-ordinator and 100 End devices, without Routers.
question was the parm Child Table Size in Network layer Configturation could not be bigger than 48. i donot know why.
was there anyway to solve my problem. thanks a lot.
i used the JN-AN-1229.
Solved! Go to Solution.
Hi,
Remember the JN5168-001-MXX has some memory size Flash 64/160/256K, so when you are join more than 48 devices, you are exceed the memory.
But, you can try with the IEEE 802.15.4 for JN516x and JN517x|NXP, if your application doesn't required Zigbee protocol.
Best Regards,
Mario
Hi,
Remember the JN5168-001-MXX has some memory size Flash 64/160/256K, so when you are join more than 48 devices, you are exceed the memory.
But, you can try with the IEEE 802.15.4 for JN516x and JN517x|NXP, if your application doesn't required Zigbee protocol.
Best Regards,
Mario
Hi
thanks a lot for your reply.
i have found JN-AN-1069,and it works very well.