JN-AN-1216-Zigbee-3-0-IoT-ControlBridge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN-AN-1216-Zigbee-3-0-IoT-ControlBridge

1,427 Views
zhijie_liang
Contributor II

Hi everybody. I have a question that when I use the newest nxp's dongle firmware whose name is ZigbeeNodeControlBridge_JN5169_FULL_FUNC_DEVICE_1000000 to the nxp dongle. When my node join the network, and send the match descriptor request with the OTA upgrade cluster, but the dongle can not send the match descriptor response, so I can not use the OTA function. And how can I fix this problem?

pastedImage_1.png

pastedImage_2.png

6 Replies

943 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liang,

What is the application note that you are working on?

Could you please provide a screen of the setting that you did? Example

pastedImage_1.png

I tried with the JN-AN-1218 Light Bulb.

Regards,

Mario

943 Views
nguyenanhgiau10
Contributor IV

I do the same your way.

But I do not see anything on Download Status.

By the way, what is WaitParams means?

Capture.PNG

0 Kudos

943 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Giam

Did you compile the AN with the OTA =1? Did you flash the bin file into the JN devices?

Example DimmableLight_GpCombo_Ota_JN5169_DR1175.bin

The wait params are not implemented.

Regards,

Mario

0 Kudos

943 Views
nguyenanhgiau10
Contributor IV

Hi Mario,

First at all, You have to burn FW DimmableLight_GpCombo_Ota_JN5169_DR1175.bin to Carrier Board.

... And using ZGWUI to permit join and OTA.

After Carrier Board joined a network from USB Dongle.

You just click "Load Image" and browse to file DimmableLight_GpCombo_Ota_JN5169_DR1175_V2.ota.

Then, just waiting and enjoy.

btw, I'm Giau, not Giam.

0 Kudos

943 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Giau,

I'm really sorry for my mistake.

Please let me know for any further question.

Regards,

Mario

0 Kudos

943 Views
nguyenanhgiau10
Contributor IV

Hi Mario,

Do you build application that have more than 1 EndPoint with OTA Upgrade?

I face this big problem. Can you help me?

0 Kudos