Importing the JN-AN-1220 appnote into BeyondStudio issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Importing the JN-AN-1220 appnote into BeyondStudio issue

Jump to solution
2,010 Views
jeanbony
Contributor II

I'm using the JN516x_EK004 kit. I have installed BeyondStudio with the following SDKs JN-SW-4168 and 4170.

All plugins for related SDKs are installed in accordance to the BeyonStudio installation guide(JN-AN-3098).

I have created a workspace and unzipped the JN-AN-1220 appnote into the workspace as described in section 5.7 in the documentation of that appnote.

Inside that workspace I have the folder 

NXP\bstudio_nxp\workspace\\JN-AN-1220-Zigbee-3-0-Sensors-v1002\

I followed the steps described in section 5.7.2.2 of the appnote document to import the appnote into BeyondStudio, but all the  sub-folders are loaded into BeyoundStudio but no source code. The folders is showing an Exclamation mark on them.

I have tried importing the zipped appnote but same result.

Any idea why I'm not able to properly load the appnote into BeyondStudio? 

I'm using BeyondStudio build 1308

0 Kudos
1 Solution
1,222 Views
jeanbony
Contributor II

Thanks for the reply. I was able to load the source file with the refresh.

However, I got a compile error when trying to compile either one of the demo apps.

I edited the following 2 Makefile options

JENNIC_CHIP?=5169 and JENNIC_CHIP_FAMILY?=516x

Then tried to build the apps, I got a " no rule to make target" error

Any idea?

beyondStudio_jn_an_1220.png

View solution in original post

0 Kudos
7 Replies
1,223 Views
jeanbony
Contributor II

Thanks for the reply. I was able to load the source file with the refresh.

However, I got a compile error when trying to compile either one of the demo apps.

I edited the following 2 Makefile options

JENNIC_CHIP?=5169 and JENNIC_CHIP_FAMILY?=516x

Then tried to build the apps, I got a " no rule to make target" error

Any idea?

beyondStudio_jn_an_1220.png

0 Kudos
1,222 Views
davidashraf
Contributor V

I think you're missing "JN" in both options 

JENNIC_CHIP ?= JN5169
JENNIC_CHIP_FAMILY ?= JN516x

0 Kudos
1,222 Views
limcb
Contributor IV

Just to check, is the path still at C:\NXP\bstudio_nxp\workspace\JN-AN-1220-Zigbee-3-0-Sensors-v1002 ?

It's searches by relative path if I'm not mistaken. 

0 Kudos
1,222 Views
jeanbony
Contributor II

I uninstall BeyondStudio and the SDKs and reinstalled everything from scratch by following the JN-AN-3098 User's guide.

I was then able to import the JN-AN-1220 source code into BeyondStudio. 

bstudio.png

Then when I tried to compile either one of the 3 apps I still got the same "No rule to make target" at the end of the build.

Also, I'm seeing all these "unresolved inclusions" in the editor for SDK (JN-SW-4170) headers, although the SDK is included in the build environment.

Here is the full build log:

11:45:03 **** Incremental Build of configuration LightTemperatureOccupancySensor for project JN-AN-1220-Zigbee-3-0-Sensors ****
make JENNIC_CHIP=JN5169 JENNIC_CHIP_FAMILY=JN516x SENSOR=LightTemperatureOccupancySensor KEEPALIVETIME=255 DR=DR1175 all
JENNIC_MAC is Mini MAC shim
Building trace version ...
rm -f bdb_DeviceCommissioning.o
rm -f bdb_fb_initiator.o
rm -f bdb_fb_common.o
rm -f bdb_ns.o
rm -f portasm.o
rm -f port.o
rm -f appZpsExtendedDebug.o
rm -f appZpsBeaconHandler.o
rm -f appZdpExtraction.o
rm -f ZTimer.o
rm -f ZQueue.o
rm -f bdb_state_machine.o
rm -f bdb_start.o
rm -f bdb_link_keys.o
rm -f bdb_fr.o
rm -f zcl_transmit.o
rm -f zcl_timer.o
rm -f zcl_search.o
rm -f zcl_reportStructure.o
rm -f zcl_reportStringHandling.o
rm -f zcl_reportScheduler.o
rm -f zcl_reportMaths.o
rm -f zcl_reportManager.o
rm -f zcl_readReportingConfigurationResponseHandle.o
rm -f zcl_readReportingConfigurationCommandSend.o
rm -f zcl_readReportingConfigurationCommandHandle.o
rm -f zcl_readAttributesResponseHandle.o
rm -f zcl_readAttributesRequestSend.o
rm -f zcl_readAttributesRequestHandle.o
rm -f zcl_library_options.o
rm -f zcl_heap.o
rm -f zcl_event.o
rm -f zcl_discoverCommandsResponseHandle.o
rm -f zcl_discoverCommandsRequestSend.o
rm -f zcl_discoverCommandsRequestHandle.o
rm -f zcl_discoverAttributesResponseHandle.o
rm -f zcl_discoverAttributesRequestSend.o
rm -f zcl_discoverAttributesRequestHandle.o
rm -f zcl_discoverAttributesExtendedResponseHandle.o
rm -f zcl_discoverAttributesExtendedRequestSend.o
rm -f zcl_discoverAttributesExtendedRequestHandle.o
rm -f zcl_defaultResponse.o
rm -f zcl_configureReportingResponseHandle.o
rm -f zcl_configureReportingCommandSend.o
rm -f zcl_configureReportingCommandHandle.o
rm -f zcl_common.o
rm -f zcl_command.o
rm -f zcl_clusterCommand.o
rm -f zcl_buffer.o
rm -f zcl_attribute.o
rm -f zcl_WriteAttributesResponseHandle.o
rm -f zcl_WriteAttributesRequestSend.o
rm -f zcl_WriteAttributesRequestHandle.o
rm -f zcl_PDUbufferReadWriteString.o
rm -f zcl_PDUbufferReadWrite.o
rm -f zcl_CustomCommandSend.o
rm -f zcl_CustomCommandReceive.o
rm -f zcl.o
rm -f dlist.o
rm -f on_off_sensor.o
rm -f on_off_plug.o
rm -f on_off_light_switch.o
rm -f on_off_light.o
rm -f on_off_ballast.o
rm -f occupancy_sensor.o
rm -f non_colour_scene_controller.o
rm -f non_colour_controller.o
rm -f light_sensor.o
rm -f light_level_sensor.o
rm -f extended_colour_light.o
rm -f dimmer_switch.o
rm -f dimmable_plug.o
rm -f dimmable_light.o
rm -f dimmable_ballast.o
rm -f control_bridge.o
rm -f commission_endpoint.o
rm -f colour_temperature_light.o
rm -f colour_scene_controller.o
rm -f colour_dimmer_switch.o
rm -f colour_dimmable_light.o
rm -f colour_controller.o
rm -f ColourControlConversions.o
rm -f ColourControlCommandHandler.o
rm -f ColourControlClientCommands.o
rm -f ColourControl.o
rm -f BallastConfiguration.o
rm -f TemperatureMeasurement.o
rm -f RelativeHumidityMeasurement.o
rm -f PressureMeasurement.o
rm -f OccupancySensing.o
rm -f IlluminanceMeasurement.o
rm -f IlluminanceLevelSensing.o
rm -f FlowMeasurement.o
rm -f ElectricalMeasurement.o
rm -f simple_sensor.o
rm -f remote_control.o
rm -f on_off_output.o
rm -f mains_power_outlet.o
rm -f base_device.o
rm -f Time.o
rm -f TC.o
rm -f ScenesTableManager.o
rm -f ScenesServerCommands.o
rm -f ScenesCommandHandler.o
rm -f ScenesClusterManagement.o
rm -f ScenesClientCommands.o
rm -f Scenes.o
rm -f PowerProfileServerCommands.o
rm -f PowerProfileCommandHandler.o
rm -f PowerProfileClientCommands.o
rm -f PowerProfile.o
rm -f PowerConfiguration.o
rm -f PollControlServerCommands.o
rm -f PollControlCommandHandler.o
rm -f PollControlClientCommands.o
rm -f PollControl.o
rm -f OnOffCommands.o
rm -f OnOffCommandHandler.o
rm -f OnOff.o
rm -f OOSC.o
rm -f MultistateOutputBasic.o
rm -f MultistateInputBasic.o
rm -f LevelControlCommandHandler.o
rm -f LevelControlClientCommands.o
rm -f LevelControl.o
rm -f IdentifyServerCommands.o
rm -f IdentifyCommandHandler.o
rm -f IdentifyClientCommands.o
rm -f Identify.o
rm -f GroupsTableManager.o
rm -f GroupsServerCommands.o
rm -f GroupsCommandHandler.o
rm -f GroupsClientCommands.o
rm -f Groups.o
rm -f Diagnostics.o
rm -f DeviceTemperatureConfiguration.o
rm -f BinaryOutputBasic.o
rm -f BinaryInputBasic.o
rm -f BasicCommandHandler.o
rm -f BasicClientCommands.o
rm -f Basic.o
rm -f AnalogOutputBasic.o
rm -f AnalogInputBasic.o
rm -f AlarmsTableManager.o
rm -f AlarmsServerCommands.o
rm -f AlarmsCommandHandler.o
rm -f AlarmsClientCommands.o
rm -f Alarms.o
rm -f app_ntag.o
rm -f app_blink_led.o
rm -f app_zcl_tick_handler.o
rm -f app_PIR_OpenCollector_events.o
rm -f app_power_on_counter.o
rm -f app_event_handler.o
rm -f app_nwk_event_handler.o
rm -f app_sleep_handler.o
rm -f app_sensor_state_machine.o
rm -f app_sensor_buttons.o
rm -f app_zcl_sensor_task.o
rm -f app_zlo_sensor_node.o
rm -f App_LightTemperatureOccupancySensor.o
rm -f app_start_sensor.o
rm -f app_main.o
rm -f app_reporting.o
rm -f app_pdm.o
rm -f zps_gen.o
rm -f pdum_apdu.o
rm -f pdum_gen.o
rm -f port_JN516x.o
rm -f portasm_JN516x.o
rm -f irq_JN516x.o
Assembling ../../LightTemperatureOccupancySensor/Source/irq_JN516x.S ...
/c/NXP/bstudio_nxp/sdk/Tools/ba-elf-ba2-r36379/bin/ba-elf-gcc -c -o ../../LightTemperatureOccupancySensor/Build/irq_JN516x.o -DSLEEP_ENABLE -DDR1175 -DLightTemperatureOccupancySensor -DBUTTON_MAP_DR1175 -DEZ_MODE_INITIATOR -DEZ_ENABLE_GROUP -DAPP_NTAG -DDBG_ENABLE -DDEBUG_SENSOR_NODE -DDEBUG_APP_NTAG -DLightTemperatureOccupancySensor -DPDM_USER_SUPPLIED_ID -DPIR_TYPE_OPEN_COLLECTOR -DJN516x=5160 -DJN5169=5169 -DJENNIC_CHIP_NAME=_JN5169 -DJENNIC_CHIP_FAMILY_NAME=_JN516x -march=ba2 -mcpu=jn51xx -mredzone-size=4 -mbranch-cost=3 -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -Wcast-align -fdata-sections -ffunction-sections -flto -DWATCHDOG_ENABLED -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DJN516X_DMA_UART_BACKWARDS_COMPATIBLE_API=1 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -DJENNIC_CHIP=JN5169 -DJENNIC_CHIP_JN5169 -DJENNIC_CHIP_FAMILY=JN516x -DJENNIC_CHIP_FAMILY_JN516x -DJENNIC_STACK_ZCL -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -I../../../../sdk/JN-SW-4170/Platform/Common/Include -DJENNIC_PCB=DEVKIT4 -DJENNIC_PCB_DEVKIT4 -I../../../../sdk/JN-SW-4170/Platform/DK4/Include -I../../../../sdk/JN-SW-4170/Components/Common/Include -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DPDM_EEPROM -DDBG_ENABLE -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZED -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_FIND_AND_BIND_INITIATOR -DBDB_SUPPORT_OOBC -I../../LightTemperatureOccupancySensor/Source -I../../LightTemperatureOccupancySensor/Source/.. -I../../Common/Source -I../../LightTemperatureOccupancySensor/Source/PIR -I../../../../sdk/JN-SW-4170/Components/ZigbeeCommon/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Include -I../../../../sdk/JN-SW-4170/Components/ZCIF/Include -I../../../../sdk/JN-SW-4170/Components/HardwareApi/Include -I../../NTAG/Include -I../../../../sdk/JN-SW-4170/Components/AppApi/Include -I../../../../sdk/JN-SW-4170/Components/MAC/Include -I../../../../sdk/JN-SW-4170/Components/MiniMac/Include -I../../../../sdk/JN-SW-4170/Components/MMAC/Include -I../../../../sdk/JN-SW-4170/Components/HardwareApi/Include -I../../../../sdk/JN-SW-4170/Components/Aes/Include -I../../../../sdk/JN-SW-4170/Components/DBG/Include -I../../../../sdk/JN-SW-4170/Components/MAC/Include -I../../../../sdk/JN-SW-4170/Components/MicroSpecific/Include -I../../../../sdk/JN-SW-4170/Components/MiniMAC/Include -I../../../../sdk/JN-SW-4170/Components/MMAC/Include -I../../../../sdk/JN-SW-4170/Components/TimerServer/Include -I../../../../sdk/JN-SW-4170/Components/Random/Include -I../../../../sdk/JN-SW-4170/Components/ZigbeeCommon/Include -I../../../../sdk/JN-SW-4170/Components/ZPSMAC_Mini/Include -I../../../../sdk/JN-SW-4170/Components/PWRM/Include -I../../../../sdk/JN-SW-4170/Components/ZPSTSV/Include -I../../../../sdk/JN-SW-4170/Components/AES_SW/Include -I../../../../sdk/JN-SW-4170/Components/PDUM/Include -I../../../../sdk/JN-SW-4170/Components/ZPSAPL/Include -I../../../../sdk/JN-SW-4170/Components/Random/Include -I../../../../sdk/JN-SW-4170/Components/PDM_EEPROM_NO_RTOS/Include -I../../../../sdk/JN-SW-4170/Components/DBG/Include -I../../../../sdk/JN-SW-4170/Components/ZPSNWK_ZED/Include -I../../../../sdk/JN-SW-4170/Components/PDM/Include -I../../../../sdk/JN-SW-4170/Components/ZPSMAC/Include -I../../../../sdk/JN-SW-4170/Components/ZPSNWK/Include -I../../../../sdk/JN-SW-4170/Components/ZCIF/Source -I../../../../sdk/JN-SW-4170/Components/ZCIF/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/General/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/General/Source -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/Lighting/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/HVAC/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/Closures/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/SecurityAndSafety/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/SmartEnergy/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/OTA/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/Commissioning/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/ApplianceManagement/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Clusters/GreenPower/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Devices/ZHA/Generic/Include -I../../../../sdk/JN-SW-4170/Components/ZCL/Devices/ZLO/Include -I../../../../sdk/JN-SW-4170/Components/BDB/Include -I../../../../sdk/JN-SW-4170/Components/BDB/Source/Common -I../../../../sdk/JN-SW-4170/Components/BDB/Source/NwkSteering -I../../../../sdk/JN-SW-4170/Components/BDB/Source/FindAndBind -I../../../../sdk/JN-SW-4170/Components/BDB/Source/OutOfBand ../../LightTemperatureOccupancySensor/Source/irq_JN516x.S -MD -MF ../../LightTemperatureOccupancySensor/Build/irq_JN516x.d -MP

make: *** No rule to make target `../../LightTemperatureOccupancySensor/Build/portasm_JN516x.o', needed by `../../LightTemperatureOccupancySensor/Build/LightTemperatureOccupancySensor_JN5169_DR1175.elf'. Stop.

11:47:25 Build Finished (took 2m:21s.833ms)

0 Kudos
1,222 Views
limcb
Contributor IV

Just to check, is your SDK installer "JN-SW-4170 Zigbee 3.0 v1518.exe" ?

0 Kudos
1,222 Views
jeanbony
Contributor II

No I was using, "JN-SW-4170 Zigbee 3.0 v1396"

I upgraded the SDK to  "JN-SW-4170 Zigbee 3.0 v1518" as per your reply and the issue is resolved.

Thank you for your help.

0 Kudos
1,222 Views
limcb
Contributor IV

Can you add a picture showing the exclamation mark ? Everything you described sounds fine. 

Can you try to right click the Project Explorer > Blue Folder icon (Project / JN-AN-1220...) and Refresh ?

0 Kudos