I2C as a slave at JN516x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C as a slave at JN516x

970 Views
ashida
Contributor I

Hello everyone,

I am trying to connect I2C as a slave at JN5164.  I describe the code shown below.  Note that an address of slave is 0x05.

 

void initialFunction(){

   vAHI_SiSlaveConfigure(0x05, FALSE, FALSE,
      E_AHI_SIS_DATA_RR_MASK |
      E_AHI_SIS_DATA_RTKN_MASK |
      E_AHI_SIS_DATA_RR_MASK |
      E_AHI_SIS_LAST_DATA_MASK |
      E_AHI_SIS_ERROR_MASK,
      FALSE);

   vAHI_SiSetLocation(FALSE);

   vAHI_SiRegisterCallback(_callbackForI2C);

   vAHI_SiSlaveWriteData8(0x30);

}

static void _callbackForI2C(uint32 u32Device, uint32 u32ItemBitmap){
   vfPrintf(&sSerStream, "Interrupted\n\r");
   vAHI_SiSlaveWriteData8(0x30);

}

 

On the other hand, a master device works well.  It can output the slave address from SDA and output clocks from SCL.  I have already checked them using an oscilloscope.  In spite of it, a bit of ACK/NACK remains high state.  It means that the slave device is not responding.

 

Does anyone has ever made a program for I2C communication in the same environment?

Thank you,

Kazuki Ashida

Labels (1)
  • JN

Tags (2)
0 Kudos
5 Replies

826 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kasuki,

What is the AN that you are working on?

Did you set up the handles interrupts priority?

For example The JN-AN-1217, the irq_JN516x.S defines the priority of the modules that you are working on. The 15 is the higher priority.

Please look at the PIC_ChannelPriorities and PIC_SwVectTable.

Hope it helps and please let me know any question that you have.

Regards,

Mario

0 Kudos

826 Views
ashida
Contributor I

Hi Mario,

Thank you for replying my message.  I use TWE-Lite which is a wireless communication module included JN-516x.  TWE-Lite is a popular module as ZigBee in Japan.  I would like to connect about 5 modules via I2C, so one module is as master and others are as slave nodes.  I don't know "JN-AN-1217", so could you tell me the relationship between JN-AN-1217 and JN516x?

Thank you,

Kazuki Ashida

0 Kudos

826 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kazuki,

I am not sure the example project that you took as reference.

The JN-AN-1217 has a file example that defines the I2C interrupts. The irq_JN516x.S file is included in that example, 

You could look at and take as a reference.

Regards,

Mario

0 Kudos

826 Views
ashida
Contributor I

Hi Mario,

I would appreciate it if you tell me the place of the example file for JN-AN-1217?  I don't know the place.

Thank you,

Kazuki Ashida

0 Kudos

826 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kasuki,

Please look at the Zigbee 3.0 JN-AN-1217

I am not sure how are you developing with the JN devices. 

Are you using the Beyond Studio IDE?

Regards,

Mario

0 Kudos