Hi All,
We are using MWPR1516 in our system. Now our customer requirement is to save parameters using the fixed-address section in MWPR1516 flash memory using the JTAG/JLINK interface.
From Segger's document, it looks like it does support such a feature. But I have done the basic experiments and when power is removed value changes to what it was earlier. I have even tried to erase the whole flash(0xFF) and tried to write 0xF9 at 0x00. But once I remove the power and again connect power 0x00 changes back to 0xFF. Please find below the procedure for the same in Jlink commander.
解決済! 解決策の投稿を見る。
We have found a way to update flash using the Write command. It turns out that if first I update the RAM Address of that variable and after that default value of that variable using the W4 command, we get the expected result.
Hi,
Pls download the WPR1516RM.pdf from the link:
https://www.nxp.com.cn/docs/en/reference-manual/WPR1516RM.pdf
The memory space from 0x0000 to 0x3FFF are flash memory(16KB).
You can not write flash as what you write RAM. If you want to program flash, pls erase the page or all flash firstly, then program the flash.
Hope it can help you
BR
XiangJun Rong
Thank you for the response.
Can you please help me with the below question?
1) Can below command be used for writing on flash(0x0000 - 0x3FFF)?
2) Can we erase one page(0x0000 - 0x0200) and rewrite whole page using Write4(W4) command?
3) Is there more steps that need to be taken to write into flash in addition to the Write4(W4) command?
We have found a way to update flash using the Write command. It turns out that if first I update the RAM Address of that variable and after that default value of that variable using the W4 command, we get the expected result.