Hello Good day,
We are doing our FCC test but having no success in doing "unmodulated signal transmission" on our DUTs? We are trying to check if we have spurious/harmonics signal. Could you please instruct us on what tools to be used and what binary files to be flash on DUT units?
Thank you
解決済! 解決策の投稿を見る。
Hi @plantze,
I hope you are doing great.
I am not sure if you are working with the FCC example that we provide in the SDK. You could find that generates the modulated or not modulated signal.
C:\NXP\QN902x_SDK_1.4.0\Projects\BLE
Please let me know if you have any further questions.
Regards,
Mario
Hi @plantze,
You are right, you are working with the correct example for the PER test, the controller.bin
Controller Mode In the Controller Mode only the link layer runs on the QN902x. The host protocol, profiles and application all run on the external microcontroller or PC. These two components communicate via HCI. Generally, this mode is not used in the product design except for the product testing. So, this example it is just for reference and doesn't provide that the device will get the certification.
I ran some test by my side and I used
Note: QN9020 can not take the tester role.
Please look at the image below, and look at the steps that I did to set the PER Test.
El KW41 has a baud rate of 115200
El QN9020 has a baud rate of 9600.
Then, you have to set the DUT and the Tester device.
Note: You have to press the reset button in the QN9020 Dev kit.
What is the Test tool Version that you have installed?
Regards,
Mario
Hello Mario,
Thank you for your immediate response. We've manage to make a DUT good for FCC/CE test.
We have another concern regarding Test Tool 12, Is it usable for QN9021?
We have tried flashing our DUTs with controller.bin and used the Test Tool 12 to do DTM PHY PER at Bluetooth LE HCI tab and Board type set to KW41Z, we were not able to make it work? Can you advise us what to do?
Hi @plantze,
I hope you are doing great.
I am not sure if you are working with the FCC example that we provide in the SDK. You could find that generates the modulated or not modulated signal.
C:\NXP\QN902x_SDK_1.4.0\Projects\BLE
Please let me know if you have any further questions.
Regards,
Mario