I have installed BeyondStudio. After that I have installed JN-SW-4168. Everytime I start the compiler, there's the error "Description Resource Path Location Type
'os_Message_zps_msgMcpsDcfm' undeclared here (not in a function) zps_gen.c /JN-AN-1189-ZigBee-HA-Demo/DimmableLight/Source line 791 C/C++ Problem".
I compare the "os_gen.h" of JN-AN-1171 and JN-AN-1189. The main difference is, that the os_Message_zps... is not defined in the JN-AN-1189, but will be used in zps_gen.c as in project JN-AN-1171.
So, what kind of changes do I have to do for a positive compiling result?
My challange is to reprogram DR1174/1175 for ZLL testing.
P.S.: I have use Index -> freshen all files already.
Hi Bjoern,
Could you please check the console log and look if the Beyond Studio is creating the bin file?
You have to save the project on the next path.
C:\NXP\bstudio_nxp\workspace
Regards,
Mario