How can I insert a NTAG in hardware? It the range damaged depending on the hardware's material?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I insert a NTAG in hardware? It the range damaged depending on the hardware's material?

377 Views
camiloa93
Contributor I

I am wondering how is functionality of the tag for it to be read with smartphones. Taking as an example smart POS systems, (contactless payments) I wonder where is the NFC tag located? I am guessing it is not a sticker but rather inserted into the hardware.

Tags (1)
0 Kudos
1 Reply

326 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I am wondering if you are looking at some device embedded with NTAG, if yes, maybe you will be interested with the following products:

LPC8N04 8 MHz |Arm® Cortex®-M0+|32-bit Microcontrollers (MCUs) | NXP 

NHS3100: NTAG SmartSensor with Temperature Sensor and Digital IOs | NXP 

NTAG 5 boost: NFC Forum-compliant I²C bridge for tiny devices | NXP 

NTAG 5 link: NFC Forum-compliant I²C bridge for IoT on demand | NXP 

NTAG 5 switch: NFC Forum-compliant PWM GPIO bridge for lighting and gaming | NXP 

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos