Hello,
I am trying to port a radio test software from JN5169 to JN5189.
On JN5169 we had the JPT.h (Production Test API) library and used following functions:
However, it seems that JPT does not exist anymore for JN5189. Which is the equivalent of JPT.h for JN5189 chip ?
Thank you,
Andrei
Hi Andri,
Unfortunately, we do not provide any reference for this. The Application Note JN-AN-1242 CMET example provides a simple document and the process of how to configure the data.
For the radio power please look at the below table for the TX power
Txpwr_Power | dBm |
-30 | -35 |
-29 | -35 |
-28 | -29 |
-27 | -29 |
-26 | -29 |
-25 | -26 |
-24 | -26 |
-23 | -25 |
-22 | -23 |
-21 | -23 |
-20 | -21 |
-19 | -21 |
-18 | -19 |
-17 | -19 |
-16 | -18 |
-15 | -16.6 |
-14 | -15.5 |
-13 | -14.8 |
-12 | -14 |
-11 | -12.5 |
-10 | -11.7 |
-9 | -10.7 |
-8 | -9.7 |
-7 | -8.7 |
-6 | -7.7 |
-5 | -6.7 |
-4 | -5.7 |
-3 | -4.7 |
-2 | -3.7 |
-1 | -2.7 |
0 | -1.7 |
1 | -0.7 |
2 | 0.3 |
3 | 1.3 |
4 | 2.3 |
5 | 3.3 |
6 | 4.3 |
7 | 5.3 |
8 | 6.3 |
9 | 7.3 |
10 | 9.5 |
Regards,
Mario
Hi Andrei,
Please look at the radio_test_jn518x.h file that includes all the APIs that you are looking for.
For example:
bool bRadio_Test_Jn518x_RadioSetChannel(uint8_t u8Channel);
uint8_t u8Radio_Test_Jn518x_RadioGetChannel(void);
uint32_t u32Radio_Test_Jn518x_Init(void);
void vRadio_Test_Jn518x_RadioSetPower(int8_t i8PowerLevel);
You could find the h file following the next path.
\JN5189DK6\middleware\wireless\framework\XCVR\DK6\Build\Include\radio_test_jn518x.h
Regards,
Mario
Hi Mario,
Thanks a lot for this.
Is there also a document describing the APIs ?
Hi Andrei,
You could find the API description on the radio.h file
\JN5189DK6\middleware\wireless\framework\XCVR\DK6\radio.h
Regards,
Mario
Hi Mario,
I was asking if there is a document(.pdf file) which describes how, when and in which order radio_test_jn518x.h APIs should be used.
For example, I would like to find out which is the maximum value of power I can set using vRadio_Test_Jn518x_RadioSetPower() function.
Thanks,
Andrei